![Logo](ti_logo.svg) |
AM263x MCU+ SDK
08.03.00
|
|
Go to the documentation of this file.
33 #ifndef UART_DMA_EDMA_H_
34 #define UART_DMA_EDMA_H_
44 typedef struct UartDma_EdmaArgs_s
Edma_IntrObject edmaIntrObjRx
Definition: uart_dma_edma.h:68
Driver implementation callbacks.
Definition: uart_dma.h:134
uint32_t edmaDummyParam
Definition: uart_dma_edma.h:62
Definition: uart_dma_edma.h:45
EDMA interrupt configuration object. The object is passed to the EDMA_registerIntr() function....
Definition: edma/v0/edma.h:449
uint32_t edmaBaseAddr
Definition: uart_dma_edma.h:66
uint32_t edmaTxParam
Definition: uart_dma_edma.h:60
Edma_IntrObject edmaIntrObjTx
Definition: uart_dma_edma.h:70
uint32_t isOpen
Definition: uart_dma_edma.h:74
uint32_t edmaRxChId
Definition: uart_dma_edma.h:54
uint32_t edmaTccDummy
Definition: uart_dma_edma.h:52
uint32_t edmaRegionId
Definition: uart_dma_edma.h:64
Edma_IntrObject edmaIntrObjDummy
Definition: uart_dma_edma.h:72
void * drvHandle
Definition: uart_dma_edma.h:46
uint32_t edmaTxChId
Definition: uart_dma_edma.h:56
uint32_t edmaTccTx
Definition: uart_dma_edma.h:50
uint32_t edmaTccRx
Definition: uart_dma_edma.h:48
uint32_t edmaRxParam
Definition: uart_dma_edma.h:58
UART_DmaFxns gUartDmaEdmaFxns