AM263x MCU+ SDK  08.03.00

Detailed Description

Icssg TX timestamp event callback info structure. This is passed to application when TX timestamp is retrieved by ICSSG driver.

Data Fields

uint32_t txTsId
 
uint64_t ts
 

Field Documentation

◆ txTsId

uint32_t Icssg_TxTsEvtCbInfo::txTsId

Timestamp Id. This was passed by an application when enabling the timestamp for the packet during EnetDma_submitTxPktQ()

◆ ts

uint64_t Icssg_TxTsEvtCbInfo::ts

Packet timestamp