Transmit Packet scatter gather list entry.
This structure contains info on scatter-gather fragments used for trasmitting packets when packets are split into list of discontinuous fragments called scatter-gather list. Each sg list has a fragment of the packet
Data Fields | |
uint8_t * | bufPtr |
uint32_t | filledLen |
bool | disableCacheOps |
uint8_t* EnetCpdma_SGListEntry::bufPtr |
Pointer to scatter fragment
uint32_t EnetCpdma_SGListEntry::filledLen |
Length of valid data in the scatter fragment
bool EnetCpdma_SGListEntry::disableCacheOps |