Go to the source code of this file.
Functions | |
int32_t | Hsmclient_loadHSMRtFirmware (const uint8_t *pHSMRt_firmware) |
Loads the HSMRt firmware. This is typically called by SBL. More... | |
int32_t | Hsmclient_init (uint32_t coreId) |
Initialize Hsm Client module. More... | |