Data Structures | |
struct | EnetTas_GenericInArgs |
Generic input args. More... | |
struct | EnetTas_GateCmdEntry |
Gate control list. See IEEE Std 802.1Q-2018 8.6.8.4. More... | |
struct | EnetTas_MaxSDUTable |
Max SDU table. See IEEE Std 802.1Q-2018 12.29.1.1. More... | |
struct | EnetTas_ControlList |
Gate control list. See IEEE Std 802.1Q-2018 8.6.9.4 D3-1. More... | |
struct | EnetTas_ConfigStatus |
Config state machine variables. See IEEE Std 802.1Q-2018 8.6.8.4. More... | |
struct | EnetTas_SetAdminListInArgs |
Input args for ENET_TAS_IOCTL_SET_ADMIN_LIST commands. More... | |
struct | EnetTas_SetStateInArgs |
Input args for ENET_TAS_IOCTL_SET_STATE commands. More... | |
Enumerations | |
enum | EnetTas_Ioctl { ENET_TAS_IOCTL_GET_VERSION = ENET_TAS_PUBLIC_IOCTL(0U), ENET_TAS_IOCTL_SET_ADMIN_LIST = ENET_TAS_PUBLIC_IOCTL(1U), ENET_TAS_IOCTL_GET_OPER_LIST_STATUS = ENET_TAS_PUBLIC_IOCTL(2U), ENET_TAS_IOCTL_SET_STATE = ENET_TAS_PUBLIC_IOCTL(3U), ENET_TAS_IOCTL_GET_STATE = ENET_TAS_PUBLIC_IOCTL(4U), ENET_TAS_IOCTL_GET_ADMIN_LIST = ENET_TAS_PUBLIC_IOCTL(5U), ENET_TAS_IOCTL_GET_OPER_LIST = ENET_TAS_PUBLIC_IOCTL(6U), ENET_TAS_IOCTL_CONFIG_CHANGE_STATUS_PARAMS = ENET_TAS_PUBLIC_IOCTL(7U) } |
TAS module IOCTL commands. More... | |
enum | EnetTas_OperStatus { ENET_TAS_OPER_LIST_NOT_YET_UPDATED = 0, ENET_TAS_OPER_LIST_UPDATED = 1 } |
TAS state types. More... | |
enum | EnetTas_TasState { ENET_TAS_DISABLE = 0, ENET_TAS_ENABLE = 1, ENET_TAS_RESET = 2 } |
TAS state types. More... | |
Macros | |
#define | ENET_TAS_PUBLIC_IOCTL(x) |
Helper macro to create IOCTL commands for TAS module. More... | |
#define | ENET_TAS_GATE_MASK(tc7, tc6, tc5, tc4, tc3, tc2, tc1, tc0) |
Helper macro to create a gate mask. More... | |
#define | ENET_TAS_MAX_CMD_LISTS (16) |
Maximum number of gate command entries in each list. More... | |
#define | ENET_TAS_MAX_NUM_QUEUES (8) |
Maximum number of transmit queues. More... | |
#define ENET_TAS_PUBLIC_IOCTL | ( | x | ) |
Helper macro to create IOCTL commands for TAS module.
#define ENET_TAS_GATE_MASK | ( | tc7, | |
tc6, | |||
tc5, | |||
tc4, | |||
tc3, | |||
tc2, | |||
tc1, | |||
tc0 | |||
) |
Helper macro to create a gate mask.
#define ENET_TAS_MAX_CMD_LISTS (16) |
Maximum number of gate command entries in each list.
#define ENET_TAS_MAX_NUM_QUEUES (8) |
Maximum number of transmit queues.
enum EnetTas_Ioctl |
TAS module IOCTL commands.
Enumerator | |
---|---|
ENET_TAS_IOCTL_GET_VERSION | Get the hardware version of the TAS module. IOCTL parameters:
Type: Synchronous. |
ENET_TAS_IOCTL_SET_ADMIN_LIST | Set the admin list parameters of the TAS module. IOCTL parameters:
Type: Asynchronous. |
ENET_TAS_IOCTL_GET_OPER_LIST_STATUS | Get the status of the operational list update. This IOCTL should be called after ENET_TAS_IOCTL_SET_ADMIN_LIST to verify admin list to operational list copy at specified time. This IOCTL should be called until ENET_TAS_OPER_LIST_UPDATED received as output. IOCTL parameters:
Type: Synchronous. |
ENET_TAS_IOCTL_SET_STATE | Set the state of the TAS module. IOCTL parameters:
Type: Asynchronous. |
ENET_TAS_IOCTL_GET_STATE | Get the state of the TAS module. IOCTL parameters:
Type: Synchronous. |
ENET_TAS_IOCTL_GET_ADMIN_LIST | Get the admin list parameters of the TAS module. IOCTL parameters:
Type: Synchronous. |
ENET_TAS_IOCTL_GET_OPER_LIST | Get the operational list parameters of the TAS module. IOCTL parameters:
Type: Synchronous. |
ENET_TAS_IOCTL_CONFIG_CHANGE_STATUS_PARAMS | Get the TAS config change status parameters. IOCTL parameters:
Type: Synchronous. |
enum EnetTas_OperStatus |
enum EnetTas_TasState |