AM263x MCU+ SDK  08.03.00
APIs for SOC Specific Functions

Introduction

For more details and example usage, see SOC

Sub Modules

 APIs for SOC Reset and Clock Functions
 
 APIs for SOC Xbars
 

Functions

int32_t SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable)
 Enable clock to specified module. More...
 
int32_t SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
 Set module clock to specified frequency. More...
 
const char * SOC_getCoreName (uint16_t coreId)
 Convert a core ID to a user readable name. More...
 
uint64_t SOC_getSelfCpuClk (void)
 Get the clock frequency in Hz of the CPU on which the driver is running. More...
 
void SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition)
 Lock control module partition to prevent writes into control MMRs. More...
 
void SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition)
 Unlock control module partition to allow writes into control MMRs. More...
 
void SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable)
 Enable or disable ePWM time base clock from Control MMR. More...
 
void SOC_enableAdcReference (uint32_t adcInstance)
 Enable ADC references by writing to Control MMR. More...
 
void SOC_setEpwmGroup (uint32_t epwmInstance, uint32_t group)
 Configure the ePWM group. More...
 
void SOC_selectSdfm1Clk0Source (uint8_t source)
 Select the SDFM1 CLK0 source. More...
 
void SOC_gateEpwmClock (uint32_t epwmInstance)
 Gate the ePWM clock. More...
 
void SOC_gateFsitxClock (uint32_t fsitxInstance)
 Gate the FSI-TX clock. More...
 
void SOC_gateFsirxClock (uint32_t fsirxInstance)
 Gate the FSI-RX clock. More...
 
void SOC_gateCmpssaClock (uint32_t cmpssaInstance)
 Gate the CMPSS-A clock. More...
 
void SOC_gateCmpssbClock (uint32_t cmpssbInstance)
 Gate the CMPSS-B clock. More...
 
void SOC_gateEcapClock (uint32_t ecapInstance)
 Gate the ECAP clock. More...
 
void SOC_gateEqepClock (uint32_t eqepInstance)
 Gate the EQEP clock. More...
 
void SOC_gateSdfmClock (uint32_t sdfmInstance)
 Gate the SDFM clock. More...
 
void SOC_gateDacClock ()
 Gate the DAC clock. More...
 
void SOC_gateAdcClock (uint32_t adcInstance)
 Gate the ADC clock. More...
 
void SOC_gateOttoClock (uint32_t ottoInstance)
 Gate the OTTO clock. More...
 
void SOC_gateSdfmPllClock (uint32_t sdfmInstance)
 Gate the SDFM PLL clock. More...
 
void SOC_gateFsiPllClock (uint32_t fsiInstance)
 Gate the FSI-TX PLL clock. More...
 
void SOC_generateEpwmReset (uint32_t ePWMInstance)
 Generate ePWM reset. More...
 
void SOC_generateFsiTxReset (uint32_t fsitxInstance)
 Generate FSI-TX reset. More...
 
void SOC_generateFsiRxReset (uint32_t fsirxInstance)
 Generate FSI-RX reset. More...
 
void SOC_generateCmpssaReset (uint32_t cmpssaInstance)
 Generate CMPSS-A reset. More...
 
void SOC_generateCmpssbReset (uint32_t cmpssbInstance)
 Generate CMPSS-B reset. More...
 
void SOC_generateEcapReset (uint32_t ecapInstance)
 Generate ECAP reset. More...
 
void SOC_generateEqepReset (uint32_t eqepInstance)
 Generate EQEP reset. More...
 
void SOC_generateSdfmReset (uint32_t sdfmInstance)
 Generate SDFM reset. More...
 
void SOC_generateDacReset ()
 Generate DAC reset. More...
 
void SOC_generateAdcReset (uint32_t adcInstance)
 Generate ADC reset. More...
 
void SOC_generateOttoReset (uint32_t ottoInstance)
 Generate OTTO reset. More...
 
void SOC_selectIcssGpiMux (uint8_t pru_instance, uint32_t mask)
 Selection of ICSS GPI MUX. More...
 
uint64_t SOC_virtToPhy (void *virtAddr)
 SOC Virtual (CPU) to Physical address translation function. More...
 
void * SOC_phyToVirt (uint64_t phyAddr)
 Physical to Virtual (CPU) address translation function. More...
 

Macros

#define MSS_CTRL_PARTITION0   (1)
 
#define TOP_CTRL_PARTITION0   (2)
 
#define CONTROLSS_CTRL_PARTITION0   (3)
 
#define MSS_RCM_PARTITION0   (4)
 
#define TOP_RCM_PARTITION0   (5)
 
#define KICK_LOCK_VAL   (0x00000000U)
 
#define KICK0_UNLOCK_VAL   (0x01234567U)
 
#define KICK1_UNLOCK_VAL   (0x0FEDCBA8U)
 

SOC Domain ID

#define SOC_DOMAIN_ID_MAIN   (0U)
 

Macro Definition Documentation

◆ SOC_DOMAIN_ID_MAIN

#define SOC_DOMAIN_ID_MAIN   (0U)

◆ MSS_CTRL_PARTITION0

#define MSS_CTRL_PARTITION0   (1)

◆ TOP_CTRL_PARTITION0

#define TOP_CTRL_PARTITION0   (2)

◆ CONTROLSS_CTRL_PARTITION0

#define CONTROLSS_CTRL_PARTITION0   (3)

◆ MSS_RCM_PARTITION0

#define MSS_RCM_PARTITION0   (4)

◆ TOP_RCM_PARTITION0

#define TOP_RCM_PARTITION0   (5)

◆ KICK_LOCK_VAL

#define KICK_LOCK_VAL   (0x00000000U)

◆ KICK0_UNLOCK_VAL

#define KICK0_UNLOCK_VAL   (0x01234567U)

◆ KICK1_UNLOCK_VAL

#define KICK1_UNLOCK_VAL   (0x0FEDCBA8U)

Function Documentation

◆ SOC_moduleClockEnable()

int32_t SOC_moduleClockEnable ( uint32_t  moduleId,
uint32_t  enable 
)

Enable clock to specified module.

Parameters
moduleId[in] see SOC_RcmPeripheralId for list of module ID's
enable[in] 1: enable clock to the module, 0: disable clock to the module
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_moduleSetClockFrequency()

int32_t SOC_moduleSetClockFrequency ( uint32_t  moduleId,
uint32_t  clkId,
uint64_t  clkRate 
)

Set module clock to specified frequency.

Parameters
moduleId[in] see SOC_RcmPeripheralId for list of module ID's
clkId[in] see SOC_RcmPeripheralClockSource for list of clocks
clkRate[in] Frequency to set in Hz
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_getCoreName()

const char* SOC_getCoreName ( uint16_t  coreId)

Convert a core ID to a user readable name.

Parameters
coreId[in] see CSL_CoreID
Returns
name as a string

◆ SOC_getSelfCpuClk()

uint64_t SOC_getSelfCpuClk ( void  )

Get the clock frequency in Hz of the CPU on which the driver is running.

Returns
Clock frequency in Hz

◆ SOC_controlModuleLockMMR()

void SOC_controlModuleLockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Lock control module partition to prevent writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_controlModuleUnlockMMR()

void SOC_controlModuleUnlockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Unlock control module partition to allow writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_setEpwmTbClk()

void SOC_setEpwmTbClk ( uint32_t  epwmInstance,
uint32_t  enable 
)

Enable or disable ePWM time base clock from Control MMR.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
enable[in] TRUE to enable and FALSE to disable

◆ SOC_enableAdcReference()

void SOC_enableAdcReference ( uint32_t  adcInstance)

Enable ADC references by writing to Control MMR.

Parameters
adcInstance[in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)]

◆ SOC_setEpwmGroup()

void SOC_setEpwmGroup ( uint32_t  epwmInstance,
uint32_t  group 
)

Configure the ePWM group.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
group[in] The group for this ePWM instance [0 - 3]

◆ SOC_selectSdfm1Clk0Source()

void SOC_selectSdfm1Clk0Source ( uint8_t  source)

Select the SDFM1 CLK0 source.

Parameters
source[in] Source of SDFM1 CLK0. 0: source is SDFM1 CK0 from Pinmux. 1: source is SDFM0 CK0 from Pinmux

◆ SOC_gateEpwmClock()

void SOC_gateEpwmClock ( uint32_t  epwmInstance)

Gate the ePWM clock.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]

◆ SOC_gateFsitxClock()

void SOC_gateFsitxClock ( uint32_t  fsitxInstance)

Gate the FSI-TX clock.

Parameters
fsitxInstance[in] FSITX instance number [0 - 3]

◆ SOC_gateFsirxClock()

void SOC_gateFsirxClock ( uint32_t  fsirxInstance)

Gate the FSI-RX clock.

Parameters
fsirxInstance[in] FSIRX instance number [0 - 3]

◆ SOC_gateCmpssaClock()

void SOC_gateCmpssaClock ( uint32_t  cmpssaInstance)

Gate the CMPSS-A clock.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_gateCmpssbClock()

void SOC_gateCmpssbClock ( uint32_t  cmpssbInstance)

Gate the CMPSS-B clock.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_gateEcapClock()

void SOC_gateEcapClock ( uint32_t  ecapInstance)

Gate the ECAP clock.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_gateEqepClock()

void SOC_gateEqepClock ( uint32_t  eqepInstance)

Gate the EQEP clock.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_gateSdfmClock()

void SOC_gateSdfmClock ( uint32_t  sdfmInstance)

Gate the SDFM clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_gateDacClock()

void SOC_gateDacClock ( )

Gate the DAC clock.

◆ SOC_gateAdcClock()

void SOC_gateAdcClock ( uint32_t  adcInstance)

Gate the ADC clock.

Parameters
adcInstance[in] ADC instance number [0 - 4]

◆ SOC_gateOttoClock()

void SOC_gateOttoClock ( uint32_t  ottoInstance)

Gate the OTTO clock.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_gateSdfmPllClock()

void SOC_gateSdfmPllClock ( uint32_t  sdfmInstance)

Gate the SDFM PLL clock.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_gateFsiPllClock()

void SOC_gateFsiPllClock ( uint32_t  fsiInstance)

Gate the FSI-TX PLL clock.

Parameters
fsiInstance[in] FSI instance number [0 - 3]

◆ SOC_generateEpwmReset()

void SOC_generateEpwmReset ( uint32_t  ePWMInstance)

Generate ePWM reset.

Parameters
ePWMInstance[in] ePWM instance number [0 - 31]

◆ SOC_generateFsiTxReset()

void SOC_generateFsiTxReset ( uint32_t  fsitxInstance)

Generate FSI-TX reset.

Parameters
fsitxInstance[in] FSI instance number [0 - 3]

◆ SOC_generateFsiRxReset()

void SOC_generateFsiRxReset ( uint32_t  fsirxInstance)

Generate FSI-RX reset.

Parameters
fsirxInstance[in] FSI instance number [0 - 3]

◆ SOC_generateCmpssaReset()

void SOC_generateCmpssaReset ( uint32_t  cmpssaInstance)

Generate CMPSS-A reset.

Parameters
cmpssaInstance[in] CMPSS-A instance number [0 - 9]

◆ SOC_generateCmpssbReset()

void SOC_generateCmpssbReset ( uint32_t  cmpssbInstance)

Generate CMPSS-B reset.

Parameters
cmpssbInstance[in] CMPSS-B instance number [0 - 9]

◆ SOC_generateEcapReset()

void SOC_generateEcapReset ( uint32_t  ecapInstance)

Generate ECAP reset.

Parameters
ecapInstance[in] ECAP instance number [0 - 9]

◆ SOC_generateEqepReset()

void SOC_generateEqepReset ( uint32_t  eqepInstance)

Generate EQEP reset.

Parameters
eqepInstance[in] EQEP instance number [0 - 2]

◆ SOC_generateSdfmReset()

void SOC_generateSdfmReset ( uint32_t  sdfmInstance)

Generate SDFM reset.

Parameters
sdfmInstance[in] SDFM instance number [0 - 1]

◆ SOC_generateDacReset()

void SOC_generateDacReset ( )

Generate DAC reset.

◆ SOC_generateAdcReset()

void SOC_generateAdcReset ( uint32_t  adcInstance)

Generate ADC reset.

Parameters
adcInstance[in] ADC instance number [0 - 4]

◆ SOC_generateOttoReset()

void SOC_generateOttoReset ( uint32_t  ottoInstance)

Generate OTTO reset.

Parameters
ottoInstance[in] OTTO instance number [0 - 3]

◆ SOC_selectIcssGpiMux()

void SOC_selectIcssGpiMux ( uint8_t  pru_instance,
uint32_t  mask 
)

Selection of ICSS GPI MUX.

Parameters
pru_instance[in] PRU instance number [0 - 1]
mask[in] Bitwise selection of ICSSM GPI source. GPI or PWMXBar select for ICSSM port 0/1. 0-GPI, 1-PWMXBAR

◆ SOC_virtToPhy()

uint64_t SOC_virtToPhy ( void *  virtAddr)

SOC Virtual (CPU) to Physical address translation function.

Parameters
virtAddr[IN] Virtual/CPU address
Returns
Corresponding SOC physical address

◆ SOC_phyToVirt()

void* SOC_phyToVirt ( uint64_t  phyAddr)

Physical to Virtual (CPU) address translation function.

Parameters
phyAddr[IN] Physical address
Returns
Corresponding virtual/CPU address