AM263x MCU+ SDK  08.03.00
DebugP.h File Reference

Go to the source code of this file.

Data Structures

struct  DebugP_ShmLog
 Data structure describing log in shared memory. More...
 

Macros

#define DebugP_SHM_LOG_SIZE   ( (2*1024U) - 16U)
 size of shared memory log for a CPU More...
 
#define DebugP_MEM_LOG_SIZE   ( 4*1024U )
 size of memory log for a CPU More...
 
#define DebugP_SHM_LOG_IS_VALID   (0x12345678U)
 Flag to indicate shared memory buffer is valid. More...
 
Debug log zones

#define DebugP_LOG_ZONE_ALWAYS_ON   (0x0001U)
 Flag for always on zone, enabled by default and recommend to not switch off. More...
 
#define DebugP_LOG_ZONE_ERROR   (0x0002U)
 Flag for error zone. More...
 
#define DebugP_LOG_ZONE_WARN   (0x0004U)
 Flag for warning zone. More...
 
#define DebugP_LOG_ZONE_INFO   (0x0008U)
 Flag for info zone. More...
 
Compile time log and assert enable, disable
#define DebugP_ASSERT_ENABLED   1
 Pre-processor define to enable or disable DebugP assert's. More...
 
#define DebugP_LOG_ENABLED   1
 Pre-processor define to enable or disable DebugP log's. More...
 
Debug assert APIs
#define DebugP_assert(expression)
 Function to call for assert check. More...
 
#define DebugP_assertNoLog(expression)   (_DebugP_assertNoLog(expression))
 Function to call for assert check, no logs are printed. More...
 
Debug log APIs
#define DebugP_log(format, ...)
 Function to log a string to the enabled console. More...
 
#define DebugP_logError(format, ...)
 Function to log a string to the enabled console, for error zone. More...
 
#define DebugP_logWarn(format, ...)
 Function to log a string to the enabled console, for warning zone. More...
 
#define DebugP_logInfo(format, ...)
 Function to log a string to the enabled console, for info zone. More...
 

Functions

void _DebugP_assert (int expression, const char *file, const char *function, int line, const char *expressionString)
 Actual function that is called for assert's by DebugP_assert. More...
 
void _DebugP_assertNoLog (int expression)
 Actual function that is called for assert's by DebugP_assertNoLog. More...
 
void _DebugP_logZone (uint32_t logZone, char *format,...)
 Function to log a string to the enabled console for a given zone. More...
 
uint32_t DebugP_logZoneEnable (uint32_t logZoneMask)
 Enable log zones. More...
 
uint32_t DebugP_logZoneDisable (uint32_t logZoneMask)
 Disable log zones. More...
 
void DebugP_logZoneRestore (uint32_t logZoneMask)
 Restire zone mask returned from DebugP_logZoneDisable or DebugP_logZoneEnable. More...
 
void DebugP_shmLogWriterInit (DebugP_ShmLog *shmLog, uint16_t selfCoreId)
 Initialize shared memory log writer for this core. More...
 
void DebugP_shmLogWriterPutChar (char character)
 Write a character to shared memory log. More...
 
void DebugP_uartLogWriterPutChar (char character)
 Write a character to UART terminal. More...
 
void DebugP_shmLogReaderInit (DebugP_ShmLog *shmLog, uint16_t numCores)
 Initialize log reader to read from shared memory and log to console via DebugP_log. More...
 
void DebugP_memLogWriterInit (uint16_t selfCoreId)
 Initialize log write to write to memory trace buffer. More...
 
void DebugP_memLogWriterPutChar (char character)
 Write a character to trace buffer. More...
 
void DebugP_uartSetDrvIndex (uint32_t uartDrvIndex)
 Set UART driver index to use for character read and write form UART. More...
 
int32_t DebugP_scanf (char *format,...)
 Read a formatted string from the selected UART driver. More...
 
int32_t DebugP_readLine (char *lineBuf, uint32_t bufSize)
 Read a string from the selected UART driver. More...