This module contains APIs to program and use the FSI TX module.
Files | |
file | fsi_tx.h |
Header file containing various enumerations, structure definitions and function declarations for the FSI TX IP. | |
Functions | |
int32_t | FSI_sendTxFlush (uint32_t base) |
This API sends FLUSH pattern. More... | |
int32_t | FSI_stopTxFlush (uint32_t base) |
This API stops FLUSH pattern transmission. More... | |
int32_t | FSI_selectTxPLLClock (uint32_t base, FSI_TxClkSel clkSel) |
This API selects PLL clock as source for clock dividers. More... | |
int32_t | FSI_enableTxClock (uint32_t base, uint16_t preScaleValue) |
This API sets clock division prescalar and enables the transmit clock. More... | |
int32_t | FSI_disableTxClock (uint32_t base) |
This API disables transmit clock. More... | |
int32_t | FSI_setTxDataWidth (uint32_t base, FSI_DataWidth dataWidth) |
This API sets Data width for transmission. More... | |
int32_t | FSI_enableTxSPIMode (uint32_t base) |
This API enables SPI compatible mode. More... | |
int32_t | FSI_disableTxSPIMode (uint32_t base) |
This API disables SPI compatible mode. More... | |
int32_t | FSI_setTxStartMode (uint32_t base, FSI_TxStartMode txStartMode) |
This API sets start mode for any frame transmission. More... | |
int32_t | FSI_setTxPingTimeoutMode (uint32_t base, FSI_PingTimeoutMode pingTimeoutMode) |
This API sets HW/SW initiated TX ping timeout mode. More... | |
int32_t | FSI_setTxExtFrameTrigger (uint32_t base, uint16_t extInputNum) |
This API sets a particular external input to trigger transmission. More... | |
int32_t | FSI_enableTxCRCForceError (uint32_t base) |
This API enables CRC value of a data frame to be forced to zero. More... | |
int32_t | FSI_disableTxCRCForceError (uint32_t base) |
This API disables forcing of CRC value of a data frame to zero. More... | |
int32_t | FSI_setTxECCComputeWidth (uint32_t base, FSI_ECCComputeWidth eccComputeWidth) |
This API select between 16-bit and 32-bit ECC computation for FSI TX. More... | |
int32_t | FSI_setTxFrameType (uint32_t base, FSI_FrameType frameType) |
This API sets frame type for transmission. More... | |
int32_t | FSI_setTxSoftwareFrameSize (uint32_t base, uint16_t nWords) |
This API sets the frame size if frame type is user/software defined frame. More... | |
int32_t | FSI_startTxTransmit (uint32_t base) |
This API starts transmitting frames. More... | |
int32_t | FSI_setTxFrameTag (uint32_t base, FSI_FrameTag frameTag) |
This API sets frame tag for transmission. More... | |
int32_t | FSI_setTxUserDefinedData (uint32_t base, uint16_t userDefData) |
This API sets user defined data for transmission It is an extra data field (8 bit) apart from regular data. More... | |
int32_t | FSI_setTxBufferPtr (uint32_t base, uint16_t bufPtrOff) |
This API sets the value for transmit buffer pointer at desired location. More... | |
int32_t | FSI_getTxBufferPtr (uint32_t base, uint16_t *pBufPtrLoc) |
This API gets current buffer pointer locationn. More... | |
int32_t | FSI_getTxWordCount (uint32_t base, uint16_t *pWordCnt) |
This API gets valid number of data words present in buffer which have not been transmitted yet. More... | |
int32_t | FSI_enableTxPingTimer (uint32_t base, uint32_t refValue, FSI_FrameTag pingFrameTag) |
This API enables ping timer logic and once set time elapses it sends signal to transmitter to send ping frame. More... | |
int32_t | FSI_setTxPingTag (uint32_t base, FSI_FrameTag frameTag) |
This API sets the ping tag value, used by either timeout counter initiated PING frame transfer or by external ping trigger input. More... | |
int32_t | FSI_disableTxPingTimer (uint32_t base) |
This API disables ping timer logic. More... | |
int32_t | FSI_enableTxExtPingTrigger (uint32_t base, uint16_t extTrigSel) |
This API enables external trigger to transmit a ping frame. More... | |
int32_t | FSI_disableTxExtPingTrigger (uint32_t base) |
This API disables external trigger logic. More... | |
int32_t | FSI_getTxCurrentPingTimeoutCounter (uint32_t base, uint32_t *pPingToCnt) |
This API gets current value of ping timeout logic counter. More... | |
int32_t | FSI_lockTxCtrl (uint32_t base) |
This API locks the control of all transmit control registers, once locked further writes will not take effect until system reset occurs. More... | |
int32_t | FSI_getTxEventStatus (uint32_t base, uint16_t *pEvtFlags) |
This API gets current status of all the error flags. More... | |
int32_t | FSI_forceTxEvents (uint32_t base, uint16_t evtFlags) |
This API enables user to set TX error flags. More... | |
int32_t | FSI_clearTxEvents (uint32_t base, uint16_t evtFlags) |
This API enables user to clear TX error flags. More... | |
int32_t | FSI_enableTxUserCRC (uint32_t base, uint16_t userCRCValue) |
This API sets the CRC value to be picked transmission if transmission is configured to use user defined SW CRC. More... | |
int32_t | FSI_disableTxUserCRC (uint32_t base) |
This API disables user defined CRC value, the transmitted CRC value is computed by hardware. More... | |
int32_t | FSI_setTxECCdata (uint32_t base, uint32_t data) |
This API sets data for ECC logic computaion. More... | |
int32_t | FSI_getTxECCValue (uint32_t base, uint16_t *pEccVal) |
This API gets ECC value evaluated for 16/32 bit data. More... | |
int32_t | FSI_enableTxInterrupt (uint32_t base, FSI_InterruptNum intNum, uint16_t intFlags) |
This API enables user to generate interrupt on occurrence of FSI_TxEventList events. More... | |
int32_t | FSI_disableTxInterrupt (uint32_t base, FSI_InterruptNum intNum, uint16_t intFlags) |
This API enables user to disable generation interrupt on occurrence of FSI TX events. More... | |
int32_t | FSI_getTxBufferAddress (uint32_t base, uint32_t *pBufAddr) |
This API gets address of TX data buffer. More... | |
int32_t | FSI_resetTxModule (uint32_t base, FSI_TxSubmoduleInReset submodule) |
This API resets clock or ping timeout counter or entire TX module. More... | |
int32_t | FSI_clearTxModuleReset (uint32_t base, FSI_TxSubmoduleInReset submodule) |
This API clears reset on clock or ping timeout counter or entire TX module. More... | |
int32_t | FSI_writeTxBuffer (uint32_t base, const uint16_t *pArray, uint16_t length, uint16_t bufOffset) |
This API writes data in FSI TX buffer. More... | |
int32_t | FSI_performTxInitialization (uint32_t base, uint16_t prescalar) |
This API initializes FSI TX module. More... | |
int32_t | FSI_executeTxFlushSequence (uint32_t base, uint16_t prescalar) |
This API sends Flush pattern sequence. More... | |
FSI TX Enum type | |
typedef uint32_t | FSI_TxEnumType |
This enumerator defines the types of possible FSI TX events. More... | |
#define | FSI_TX_EVT_FRAME_DONE ((uint16_t)0x1U) |
#define | FSI_TX_EVT_BUF_UNDERRUN ((uint16_t)0x2U) |
#define | FSI_TX_EVT_BUF_OVERRUN ((uint16_t)0x4U) |
#define | FSI_TX_EVT_PING_TIMEOUT ((uint16_t)0x8U) |
#define | FSI_TX_EVT_PING_HW_TRIG ((uint16_t)0x8U) |
#define | FSI_TX_EVTMASK ((uint16_t)0xFU) |
Mask of all TX Event types. More... | |
#define | FSI_TX_MAX_NUM_EXT_TRIGGERS ((uint16_t)0x20U) |
maximum number of external input for triggering frame-transmission More... | |
#define | FSI_TX_INT2_CTRL_S ((uint16_t)0x8U) |
Shifts needed to control FSI TX interrupt generation on INT2. More... | |
FSI TX submodules can be in reset | |
typedef uint32_t | FSI_TxSubmoduleInReset |
TX submodules that can be reset with reset APIs. More... | |
#define | FSI_TX_MASTER_CORE_RESET ((uint32_t)0x0U) |
#define | FSI_TX_CLOCK_RESET ((uint32_t)0x1U) |
#define | FSI_TX_PING_TIMEOUT_CNT_RESET ((uint32_t)0x2U) |
FSI TX start mode | |
typedef uint32_t | FSI_TxStartMode |
Start Mode for TX frame transmission (i.e. how transmission will start) More... | |
#define | FSI_TX_START_FRAME_CTRL ((uint32_t)0x0U) |
#define | FSI_TX_START_EXT_TRIG ((uint32_t)0x1U) |
#define | FSI_TX_START_FRAME_CTRL_OR_UDATA_TAG ((uint32_t)0x2U) |
FSI TX input clock select | |
typedef uint32_t | FSI_TxClkSel |
FSI TX input clock select. More... | |
#define | FSI_TX_CLK_SEL0 ((uint32_t)0x0U) |
#define | FSI_TX_CLK_SEL1 ((uint32_t)0x1U) |
FSI frame tag | |
typedef uint32_t | FSI_FrameTag |
FSI frame tag values. More... | |
#define | FSI_FRAME_TAG0 ((uint32_t)0x0U) |
#define | FSI_FRAME_TAG1 ((uint32_t)0x1U) |
#define | FSI_FRAME_TAG2 ((uint32_t)0x2U) |
#define | FSI_FRAME_TAG3 ((uint32_t)0x3U) |
#define | FSI_FRAME_TAG4 ((uint32_t)0x4U) |
#define | FSI_FRAME_TAG5 ((uint32_t)0x5U) |
#define | FSI_FRAME_TAG6 ((uint32_t)0x6U) |
#define | FSI_FRAME_TAG7 ((uint32_t)0x7U) |
#define | FSI_FRAME_TAG8 ((uint32_t)0x8U) |
#define | FSI_FRAME_TAG9 ((uint32_t)0x9U) |
#define | FSI_FRAME_TAG10 ((uint32_t)0xAU) |
#define | FSI_FRAME_TAG11 ((uint32_t)0xBU) |
#define | FSI_FRAME_TAG12 ((uint32_t)0xCU) |
#define | FSI_FRAME_TAG13 ((uint32_t)0xDU) |
#define | FSI_FRAME_TAG14 ((uint32_t)0xEU) |
#define | FSI_FRAME_TAG15 ((uint32_t)0xFU) |
#define FSI_TX_EVT_FRAME_DONE ((uint16_t)0x1U) |
#define FSI_TX_EVT_BUF_UNDERRUN ((uint16_t)0x2U) |
TX frame done event
#define FSI_TX_EVT_BUF_OVERRUN ((uint16_t)0x4U) |
TX buffer underrun event
#define FSI_TX_EVT_PING_TIMEOUT ((uint16_t)0x8U) |
TX buffer overrun event
#define FSI_TX_EVT_PING_HW_TRIG ((uint16_t)0x8U) |
TX ping timeout event
#define FSI_TX_EVTMASK ((uint16_t)0xFU) |
Mask of all TX Event types.
TX ping hardware trigger event
#define FSI_TX_MAX_NUM_EXT_TRIGGERS ((uint16_t)0x20U) |
maximum number of external input for triggering frame-transmission
#define FSI_TX_INT2_CTRL_S ((uint16_t)0x8U) |
Shifts needed to control FSI TX interrupt generation on INT2.
#define FSI_TX_MASTER_CORE_RESET ((uint32_t)0x0U) |
Reset entire TX Module
#define FSI_TX_CLOCK_RESET ((uint32_t)0x1U) |
Reset only TX clock
#define FSI_TX_PING_TIMEOUT_CNT_RESET ((uint32_t)0x2U) |
Reset ping timeout counter
#define FSI_TX_START_FRAME_CTRL ((uint32_t)0x0U) |
SW write of START bit in TX_PKT_CTRL register
#define FSI_TX_START_EXT_TRIG ((uint32_t)0x1U) |
Rising edge on external trigger
#define FSI_TX_START_FRAME_CTRL_OR_UDATA_TAG ((uint32_t)0x2U) |
Either SW write of START bit or Frame completion
#define FSI_TX_CLK_SEL0 ((uint32_t)0x0U) |
Input clock select 0
#define FSI_TX_CLK_SEL1 ((uint32_t)0x1U) |
Input clock select 1
#define FSI_FRAME_TAG0 ((uint32_t)0x0U) |
Frame tag value 0
#define FSI_FRAME_TAG1 ((uint32_t)0x1U) |
Frame tag value 1
#define FSI_FRAME_TAG2 ((uint32_t)0x2U) |
Frame tag value 2
#define FSI_FRAME_TAG3 ((uint32_t)0x3U) |
Frame tag value 3
#define FSI_FRAME_TAG4 ((uint32_t)0x4U) |
Frame tag value 4
#define FSI_FRAME_TAG5 ((uint32_t)0x5U) |
Frame tag value 5
#define FSI_FRAME_TAG6 ((uint32_t)0x6U) |
Frame tag value 6
#define FSI_FRAME_TAG7 ((uint32_t)0x7U) |
Frame tag value 7
#define FSI_FRAME_TAG8 ((uint32_t)0x8U) |
Frame tag value 8
#define FSI_FRAME_TAG9 ((uint32_t)0x9U) |
Frame tag value 9
#define FSI_FRAME_TAG10 ((uint32_t)0xAU) |
Frame tag value 10
#define FSI_FRAME_TAG11 ((uint32_t)0xBU) |
Frame tag value 11
#define FSI_FRAME_TAG12 ((uint32_t)0xCU) |
Frame tag value 12
#define FSI_FRAME_TAG13 ((uint32_t)0xDU) |
Frame tag value 13
#define FSI_FRAME_TAG14 ((uint32_t)0xEU) |
Frame tag value 14
#define FSI_FRAME_TAG15 ((uint32_t)0xFU) |
Frame tag value 15
typedef uint32_t FSI_TxEnumType |
This enumerator defines the types of possible FSI TX events.
Values that can be passed to APIs to enable/disable interrupts and also to set/get/clear event status on FSI TX operation.
There are 4 supported interrupts related to TX events, all are available as event status as well excecpt 4th one. 1) frame transmission done 2) transmit buffer is underrun 3) transmit buffer is overrun 4) ping counter timeout
Ping frame transmission upon hardware trigger (ping watchdog or external trigger) is shown as event status.
typedef uint32_t FSI_TxSubmoduleInReset |
TX submodules that can be reset with reset APIs.
typedef uint32_t FSI_TxStartMode |
Start Mode for TX frame transmission (i.e. how transmission will start)
typedef uint32_t FSI_TxClkSel |
FSI TX input clock select.
typedef uint32_t FSI_FrameTag |
FSI frame tag values.
4 bit field inside FSI frame is available to set tag value (0-15)
int32_t FSI_sendTxFlush | ( | uint32_t | base | ) |
This API sends FLUSH pattern.
FLUSH pattern (toggle data lines followed by toggle on clocks) should be sent only when FSI TX is not under SOFT_RESET and the clock to the transmit core has been turned ON.
base | [IN] Base address of the FSI TX module |
int32_t FSI_stopTxFlush | ( | uint32_t | base | ) |
This API stops FLUSH pattern transmission.
Transmission of FLUSH pattern should be stopped before starting sending frames. Generally during initilization a pair of send/stop APIs for FLUSH pattern is called to clear data/clock lines.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_selectTxPLLClock | ( | uint32_t | base, |
FSI_TxClkSel | clkSel | ||
) |
This API selects PLL clock as source for clock dividers.
base | [IN] Base address of the FSI TX module. |
clkSel | [IN] Input PLL clock select to the FSI TX module refer FSI_TxClkSel. |
int32_t FSI_enableTxClock | ( | uint32_t | base, |
uint16_t | preScaleValue | ||
) |
This API sets clock division prescalar and enables the transmit clock.
base | [IN] Base address of the FSI TX module. |
preScaleValue | [IN] prescale value used to generate transmit clock, it defines the division value of /2,/3,/4, etc. of PLL CLK |
int32_t FSI_disableTxClock | ( | uint32_t | base | ) |
This API disables transmit clock.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_setTxDataWidth | ( | uint32_t | base, |
FSI_DataWidth | dataWidth | ||
) |
This API sets Data width for transmission.
base | [IN] Base address of the FSI TX module. |
dataWidth | [IN] Data lines used for TX operation refer FSI_DataWidth. |
int32_t FSI_enableTxSPIMode | ( | uint32_t | base | ) |
This API enables SPI compatible mode.
This API is only applicable when communicating with a SPI interface
FSI supports a compatibility mode in order to communicate with legacy peripherals like SPI. Only the 16-bit mode of SPI will be supported. All the frame structures, CRC checks and will be identical to the normal FSI frames.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_disableTxSPIMode | ( | uint32_t | base | ) |
This API disables SPI compatible mode.
This API is only applicable when communicating with a SPI interface
base | [IN] Base address of the FSI TX module. |
int32_t FSI_setTxStartMode | ( | uint32_t | base, |
FSI_TxStartMode | txStartMode | ||
) |
This API sets start mode for any frame transmission.
base | [IN] Base address of the FSI TX module. |
txStartMode | [IN] Refer FSI_TxStartMode |
int32_t FSI_setTxPingTimeoutMode | ( | uint32_t | base, |
FSI_PingTimeoutMode | pingTimeoutMode | ||
) |
This API sets HW/SW initiated TX ping timeout mode.
base | [IN] Base address of the FSI TX module. |
pingTimeoutMode | [IN] Refer FSI_PingTimeoutMode |
int32_t FSI_setTxExtFrameTrigger | ( | uint32_t | base, |
uint16_t | extInputNum | ||
) |
This API sets a particular external input to trigger transmission.
base | [IN] Base address of the FSI TX module. |
extInputNum | [IN] external input number, from 0 to 31 |
int32_t FSI_enableTxCRCForceError | ( | uint32_t | base | ) |
This API enables CRC value of a data frame to be forced to zero.
CRC value of the data frame will be forced to 0 whenever there is a transmission and buffer over-run or under-run condition happens. The idea is to force a corruption of the CRC since the data is not guaranteed to be reliable
base | [IN] Base address of the FSI TX module. |
int32_t FSI_disableTxCRCForceError | ( | uint32_t | base | ) |
This API disables forcing of CRC value of a data frame to zero.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_setTxECCComputeWidth | ( | uint32_t | base, |
FSI_ECCComputeWidth | eccComputeWidth | ||
) |
This API select between 16-bit and 32-bit ECC computation for FSI TX.
base | [IN] Base address of the FSI TX module. |
eccComputeWidth | [IN] Refer FSI_ECCComputeWidth |
int32_t FSI_setTxFrameType | ( | uint32_t | base, |
FSI_FrameType | frameType | ||
) |
This API sets frame type for transmission.
base | [IN] Base address of the FSI TX module. |
frameType | [IN] Refer FSI_FrameType |
int32_t FSI_setTxSoftwareFrameSize | ( | uint32_t | base, |
uint16_t | nWords | ||
) |
This API sets the frame size if frame type is user/software defined frame.
base | [IN] Base address of the FSI TX module. |
nWords | [IN] number of data words in a software defined frame |
int32_t FSI_startTxTransmit | ( | uint32_t | base | ) |
This API starts transmitting frames.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_setTxFrameTag | ( | uint32_t | base, |
FSI_FrameTag | frameTag | ||
) |
This API sets frame tag for transmission.
base | [IN] Base address of the FSI TX module. |
frameTag | [IN] refer FSI_FrameTag |
int32_t FSI_setTxUserDefinedData | ( | uint32_t | base, |
uint16_t | userDefData | ||
) |
This API sets user defined data for transmission It is an extra data field (8 bit) apart from regular data.
base | [IN] Base address of the FSI TX module. |
userDefData | [IN] 8 bit user defined data value |
int32_t FSI_setTxBufferPtr | ( | uint32_t | base, |
uint16_t | bufPtrOff | ||
) |
This API sets the value for transmit buffer pointer at desired location.
base | [IN] Base address of the FSI TX module. |
bufPtrOff | [IN] 4 bit offset pointer in TX buffer where transmitter will pick the data |
int32_t FSI_getTxBufferPtr | ( | uint32_t | base, |
uint16_t * | pBufPtrLoc | ||
) |
This API gets current buffer pointer locationn.
base | [IN] Base address of the FSI TX module. |
pBufPtrLoc | [OUT] Pointer to current buffer pointer location |
int32_t FSI_getTxWordCount | ( | uint32_t | base, |
uint16_t * | pWordCnt | ||
) |
This API gets valid number of data words present in buffer which have not been transmitted yet.
there could be lag due to synchronization hence value is accurate only when no current transmission is happening
base | [IN] Base address of the FSI TX module. |
pWordCnt | [OUT] Pointer to number of data words |
int32_t FSI_enableTxPingTimer | ( | uint32_t | base, |
uint32_t | refValue, | ||
FSI_FrameTag | pingFrameTag | ||
) |
This API enables ping timer logic and once set time elapses it sends signal to transmitter to send ping frame.
there could be lag due to synchronization hence value is accurate only when no current transmission is happening
base | [IN] Base address of the FSI TX module. |
refValue | [IN] 32 bit reference value for ping time-out counter |
pingFrameTag | [IN] 4 bit tag value for ping time-out counter refer FSI_FrameTag |
int32_t FSI_setTxPingTag | ( | uint32_t | base, |
FSI_FrameTag | frameTag | ||
) |
This API sets the ping tag value, used by either timeout counter initiated PING frame transfer or by external ping trigger input.
base | [IN] Base address of the FSI TX module. |
frameTag | [IN] 4 bit tag value for ping time-out counter refer FSI_FrameTag |
int32_t FSI_disableTxPingTimer | ( | uint32_t | base | ) |
This API disables ping timer logic.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_enableTxExtPingTrigger | ( | uint32_t | base, |
uint16_t | extTrigSel | ||
) |
This API enables external trigger to transmit a ping frame.
base | [IN] Base address of the FSI TX module. |
extTrigSel | [IN] 5 bit value which selects among 32 external inputs |
int32_t FSI_disableTxExtPingTrigger | ( | uint32_t | base | ) |
This API disables external trigger logic.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_getTxCurrentPingTimeoutCounter | ( | uint32_t | base, |
uint32_t * | pPingToCnt | ||
) |
This API gets current value of ping timeout logic counter.
base | [IN] Base address of the FSI TX module. |
pPingToCnt | [OUT] Pointer to current ping timeout counter |
int32_t FSI_lockTxCtrl | ( | uint32_t | base | ) |
This API locks the control of all transmit control registers, once locked further writes will not take effect until system reset occurs.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_getTxEventStatus | ( | uint32_t | base, |
uint16_t * | pEvtFlags | ||
) |
This API gets current status of all the error flags.
base | [IN] Base address of the FSI TX module. |
pEvtFlags | [OUT] Pointer to the status of error event flags, each bit of integer is associated with one error flag. |
int32_t FSI_forceTxEvents | ( | uint32_t | base, |
uint16_t | evtFlags | ||
) |
This API enables user to set TX error flags.
base | [IN] Base address of the FSI TX module. |
evtFlags | [IN] event and error flags to be set |
Writing a 1 to this bit position will cause the corresponding bit in TX_EVT_ERR_STATUS register to get set. The purpose of this register is to allow software to simulate the effect of the event and test the associated software/ISR.
int32_t FSI_clearTxEvents | ( | uint32_t | base, |
uint16_t | evtFlags | ||
) |
This API enables user to clear TX error flags.
base | [IN] Base address of the FSI TX module. |
evtFlags | [IN] event and error flags to be cleared |
Writing a 1 to this bit position will cause the corresponding bit in TX_EVT_ERR_STATUS register to get cleared to 0.
int32_t FSI_enableTxUserCRC | ( | uint32_t | base, |
uint16_t | userCRCValue | ||
) |
This API sets the CRC value to be picked transmission if transmission is configured to use user defined SW CRC.
base | [IN] Base address of the FSI TX module. |
userCRCValue | [IN] user defined CRC value |
int32_t FSI_disableTxUserCRC | ( | uint32_t | base | ) |
This API disables user defined CRC value, the transmitted CRC value is computed by hardware.
base | [IN] Base address of the FSI TX module. |
int32_t FSI_setTxECCdata | ( | uint32_t | base, |
uint32_t | data | ||
) |
This API sets data for ECC logic computaion.
base | [IN] Base address of the FSI TX module. |
data | [IN] data value for which ECC needs to be computed |
int32_t FSI_getTxECCValue | ( | uint32_t | base, |
uint16_t * | pEccVal | ||
) |
This API gets ECC value evaluated for 16/32 bit data.
base | [IN] Base address of the FSI TX module. |
pEccVal | [OUT] Pointer to the ECC value for input data. |
int32_t FSI_enableTxInterrupt | ( | uint32_t | base, |
FSI_InterruptNum | intNum, | ||
uint16_t | intFlags | ||
) |
This API enables user to generate interrupt on occurrence of FSI_TxEventList events.
base | [IN] Base address of the FSI TX module. |
intNum | [IN] Type of interrupt to be generated, INT1 or INT2 |
intFlags | [IN] TX events on which interrupt should be generated |
int32_t FSI_disableTxInterrupt | ( | uint32_t | base, |
FSI_InterruptNum | intNum, | ||
uint16_t | intFlags | ||
) |
This API enables user to disable generation interrupt on occurrence of FSI TX events.
base | [IN] Base address of the FSI TX module. |
intNum | [IN] Type of interrupt to be generated, INT1 or INT2 |
intFlags | [IN] TX events on which interrupt generation has to be disabled |
int32_t FSI_getTxBufferAddress | ( | uint32_t | base, |
uint32_t * | pBufAddr | ||
) |
This API gets address of TX data buffer.
Data buffer is consisting of 16 words from offset- 0x40 to 0x4e
base | [IN] Base address of the FSI TX module. |
pBufAddr | [OUT] Pointer to the TX data buffer address |
int32_t FSI_resetTxModule | ( | uint32_t | base, |
FSI_TxSubmoduleInReset | submodule | ||
) |
This API resets clock or ping timeout counter or entire TX module.
base | [IN] Base address of the FSI TX module. |
submodule | [IN] name of submodule which is supposed to be reset |
int32_t FSI_clearTxModuleReset | ( | uint32_t | base, |
FSI_TxSubmoduleInReset | submodule | ||
) |
This API clears reset on clock or ping timeout counter or entire TX module.
base | [IN] Base address of the FSI TX module. |
submodule | [IN] name of submodule to be brought out of reset |
int32_t FSI_writeTxBuffer | ( | uint32_t | base, |
const uint16_t * | pArray, | ||
uint16_t | length, | ||
uint16_t | bufOffset | ||
) |
This API writes data in FSI TX buffer.
base | [IN] Base address of the FSI TX module. |
pArray | [IN] Address of the array of words to be transmitted. |
length | [IN] Length is the number of words in the array to be transmitted. |
bufOffset | [IN] Offset in TX buffer where data will be written, offset is a 16-bit aligned address |
int32_t FSI_performTxInitialization | ( | uint32_t | base, |
uint16_t | prescalar | ||
) |
This API initializes FSI TX module.
Software based initialization of the FSI transmitter IP. This is typically needed only once during initialization or if the module needs to be reset due to an underrun condition that occurred during operation.
base | [IN] Base address of the FSI TX module |
prescalar | [IN] User configurable clock divider for PLL input clock |
int32_t FSI_executeTxFlushSequence | ( | uint32_t | base, |
uint16_t | prescalar | ||
) |
This API sends Flush pattern sequence.
Flush pattern sequence sent by a FSI transmit module will bring the FSI receive module out of reset so that it will then be ready to receive subsequent frames.
base | [IN] Base address of the FSI TX module |
prescalar | [IN] user configurable clock divider for PLL input clock |