Values that can be passed to SDFM_configCompEventLowFilter() & SDFM_configCompEventHighFilter() as the filterNumber.
Data Fields | |
uint16_t | sampleWindow |
Sample window size. More... | |
uint16_t | threshold |
Majority voting threshold. More... | |
uint16_t | clkPrescale |
Sample clock pre-scale. More... | |
uint16_t SDFM_CompEventFilterConfig::sampleWindow |
Sample window size.
uint16_t SDFM_CompEventFilterConfig::threshold |
Majority voting threshold.
uint16_t SDFM_CompEventFilterConfig::clkPrescale |
Sample clock pre-scale.