MCSPI Parameters.
MCSPI Parameters are used to with the MCSPI_open() call. Default values for these parameters are set using MCSPI_OpenParams_init().
If NULL is passed for the parameters, MCSPI_open() uses default parameters.
Data Fields | |
uint32_t | transferMode |
uint32_t | transferTimeout |
MCSPI_CallbackFxn | transferCallbackFxn |
uint32_t | msMode |
uint32_t MCSPI_OpenParams::transferMode |
Blocking or Callback mode. Refer MCSPI_TransferMode
uint32_t MCSPI_OpenParams::transferTimeout |
Transfer timeout in system ticks
MCSPI_CallbackFxn MCSPI_OpenParams::transferCallbackFxn |
Callback function pointer
uint32_t MCSPI_OpenParams::msMode |
Master or Slave mode. Refer MCSPI_MsMode