|
typedef void(* | RPMessage_RecvCallback) (RPMessage_Object *obj, void *arg, void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt) |
| Callback that is invoked when a message is received from any CPU at the specified local end point. More...
|
|
typedef void(* | RPMessage_RecvNotifyCallback) (RPMessage_Object *obj, void *arg) |
| Callback that is invoked when a message is received from any CPU at the specified local end point. More...
|
|
typedef void(* | RPMessage_ControlEndPtCallback) (void *arg, uint16_t remoteCoreId, uint16_t remoteEndPt, const char *remoteServiceName) |
| Callback that is invoked when a annoucement message is received on the control end point. More...
|
|
|
void | RPMessage_Params_init (RPMessage_Params *params) |
| Set default values to RPMessage_Params. More...
|
|
void | RPMessage_CreateParams_init (RPMessage_CreateParams *params) |
| Set default values to RPMessage_CreateParams. More...
|
|
int32_t | RPMessage_init (const RPMessage_Params *params) |
| Initialize RPMessage module. More...
|
|
void | RPMessage_deInit () |
| De-Initialize RPMessage module. More...
|
|
int32_t | RPMessage_waitForLinuxReady (uint32_t timeout) |
| Wait for linux side RPMessage to be ready. More...
|
|
void | RPMessage_controlEndPtCallback (RPMessage_ControlEndPtCallback controlEndPtCallback, void *controlEndPtCallbackArgs) |
| Callback to call when a control message is received on a control end point. More...
|
|
int32_t | RPMessage_construct (RPMessage_Object *obj, const RPMessage_CreateParams *createParams) |
| Create a RPMessage object to receive messages at a specified end-point. More...
|
|
void | RPMessage_destruct (RPMessage_Object *obj) |
| Delete a previously created RPMessage object. More...
|
|
void | RPMessage_unblock (RPMessage_Object *obj) |
| Unblocks RPMessage_recv, for the input object, if it is blocked waiting on messages and users want to exit that task. More...
|
|
uint16_t | RPMessage_getLocalEndPt (const RPMessage_Object *obj) |
| Return local end point of a RPMessage_Object. More...
|
|
int32_t | RPMessage_announce (uint16_t remoteProcId, uint16_t localEndPt, const char *name) |
| Announce a local end point at which a service is created to a remote core. More...
|
|
int32_t | RPMessage_send (void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt, uint16_t localEndPt, uint32_t timeout) |
| Send a message to a remote core at a specified remote end point. More...
|
|
int32_t | RPMessage_recv (RPMessage_Object *obj, void *data, uint16_t *dataLen, uint16_t *remoteCoreId, uint16_t *remoteEndPt, uint32_t timeout) |
| Blocking API to wait till a message is received from any CPU at the specified local end point. More...
|
|