This module contains APIs to program and use the EQEP module.
Data Structures | |
struct | EQEP_SourceSelect |
Functions | |
static void | EQEP_enableModule (uint32_t base) |
static void | EQEP_disableModule (uint32_t base) |
static void | EQEP_setDecoderConfig (uint32_t base, uint16_t config) |
static void | EQEP_setPositionCounterConfig (uint32_t base, EQEP_PositionResetMode mode, uint32_t maxPosition) |
static uint32_t | EQEP_getPosition (uint32_t base) |
static void | EQEP_setPosition (uint32_t base, uint32_t position) |
static int16_t | EQEP_getDirection (uint32_t base) |
static void | EQEP_enableInterrupt (uint32_t base, uint16_t intFlags) |
static void | EQEP_disableInterrupt (uint32_t base, uint16_t intFlags) |
static uint16_t | EQEP_getInterruptStatus (uint32_t base) |
static void | EQEP_clearInterruptStatus (uint32_t base, uint16_t intFlags) |
static void | EQEP_forceInterrupt (uint32_t base, uint16_t intFlags) |
static bool | EQEP_getError (uint32_t base) |
static uint16_t | EQEP_getStatus (uint32_t base) |
static void | EQEP_clearStatus (uint32_t base, uint16_t statusFlags) |
static void | EQEP_setCaptureConfig (uint32_t base, EQEP_CAPCLKPrescale capPrescale, EQEP_UPEVNTPrescale evntPrescale) |
static void | EQEP_enableCapture (uint32_t base) |
static void | EQEP_disableCapture (uint32_t base) |
static uint16_t | EQEP_getCapturePeriod (uint32_t base) |
static uint16_t | EQEP_getCaptureTimer (uint32_t base) |
static void | EQEP_enableCompare (uint32_t base) |
static void | EQEP_disableCompare (uint32_t base) |
static void | EQEP_setComparePulseWidth (uint32_t base, uint16_t cycles) |
static void | EQEP_loadUnitTimer (uint32_t base, uint32_t period) |
static void | EQEP_enableUnitTimer (uint32_t base, uint32_t period) |
static void | EQEP_disableUnitTimer (uint32_t base) |
static void | EQEP_enableWatchdog (uint32_t base, uint16_t period) |
static void | EQEP_disableWatchdog (uint32_t base) |
static void | EQEP_setWatchdogTimerValue (uint32_t base, uint16_t value) |
static uint16_t | EQEP_getWatchdogTimerValue (uint32_t base) |
static void | EQEP_setPositionInitMode (uint32_t base, uint16_t initMode) |
static void | EQEP_setSWPositionInit (uint32_t base, bool initialize) |
static void | EQEP_setInitialPosition (uint32_t base, uint32_t position) |
static void | EQEP_setLatchMode (uint32_t base, uint32_t latchMode) |
static uint32_t | EQEP_getIndexPositionLatch (uint32_t base) |
static uint32_t | EQEP_getStrobePositionLatch (uint32_t base) |
static uint32_t | EQEP_getPositionLatch (uint32_t base) |
static uint16_t | EQEP_getCaptureTimerLatch (uint32_t base) |
static uint16_t | EQEP_getCapturePeriodLatch (uint32_t base) |
static void | EQEP_setQMAModuleMode (uint32_t base, EQEP_QMAMode qmaMode) |
static void | EQEP_setStrobeSource (uint32_t base, EQEP_StrobeSource strobeSrc) |
static void | EQEP_enableDirectionChangeDuringIndex (uint32_t base) |
static void | EQEP_disableDirectionChangeDuringIndex (uint32_t base) |
static void | EQEP_selectSource (uint32_t base, EQEP_SourceSelect sourceConfig) |
static void | EQEP_setEmulationMode (uint32_t base, EQEP_EmulationMode emuMode) |
void | EQEP_setCompareConfig (uint32_t base, uint16_t config, uint32_t compareValue, uint16_t cycles) |
void | EQEP_setInputPolarity (uint32_t base, bool invertQEPA, bool invertQEPB, bool invertIndex, bool invertStrobe) |
Macros | |
#define | EQEP_CONFIG_QUADRATURE (0x0000U) |
Header files. More... | |
#define | EQEP_CONFIG_CLOCK_DIR (0x4000U) |
Up-count mode, QDIR = 1. More... | |
#define | EQEP_CONFIG_UP_COUNT (0x8000U) |
Down-count mode, QDIR = 0. More... | |
#define | EQEP_CONFIG_DOWN_COUNT (0xC000U) |
#define | EQEP_CONFIG_2X_RESOLUTION (0x0000U) |
< Count rising and falling edge More... | |
#define | EQEP_CONFIG_1X_RESOLUTION (0x0800U) |
#define | EQEP_CONFIG_NO_SWAP (0x0000U) |
< Do not swap QEPA and QEPB More... | |
#define | EQEP_CONFIG_SWAP (0x0400U) |
#define | EQEP_COMPARE_NO_SYNC_OUT (0x0000U) |
< Disable sync output More... | |
#define | EQEP_COMPARE_IDX_SYNC_OUT (0x2000U) |
Sync output on strobe pin. More... | |
#define | EQEP_COMPARE_STROBE_SYNC_OUT (0x3000U) |
#define | EQEP_COMPARE_NO_SHADOW (0x0000U) |
< Disable shadow of QPOSCMP More... | |
#define | EQEP_COMPARE_LOAD_ON_ZERO (0x8000U) |
Load on QPOSCNT = QPOSCMP. More... | |
#define | EQEP_COMPARE_LOAD_ON_MATCH (0xC000U) |
#define | EQEP_INT_GLOBAL (0x0001U) |
Global interrupt flag. More... | |
#define | EQEP_INT_POS_CNT_ERROR (0x0002U) |
Position counter error. More... | |
#define | EQEP_INT_PHASE_ERROR (0x0004U) |
Quadrature phase error. More... | |
#define | EQEP_INT_DIR_CHANGE (0x0008U) |
Quadrature direction change. More... | |
#define | EQEP_INT_WATCHDOG (0x0010U) |
Watchdog time-out. More... | |
#define | EQEP_INT_UNDERFLOW (0x0020U) |
Position counter underflow. More... | |
#define | EQEP_INT_OVERFLOW (0x0040U) |
Position counter overflow. More... | |
#define | EQEP_INT_POS_COMP_READY (0x0080U) |
Position-compare ready. More... | |
#define | EQEP_INT_POS_COMP_MATCH (0x0100U) |
Position-compare match. More... | |
#define | EQEP_INT_STROBE_EVNT_LATCH (0x0200U) |
Strobe event latch. More... | |
#define | EQEP_INT_INDEX_EVNT_LATCH (0x0400U) |
Index event latch. More... | |
#define | EQEP_INT_UNIT_TIME_OUT (0x0800U) |
Unit time-out. More... | |
#define | EQEP_INT_QMA_ERROR (0x1000U) |
QMA error. More... | |
#define | EQEP_STS_UNIT_POS_EVNT (0x0080U) |
Unit position event detected. More... | |
#define | EQEP_STS_DIR_ON_1ST_IDX (0x0040U) |
Direction was clockwise on first index event. More... | |
#define | EQEP_STS_DIR_FLAG (0x0020U) |
Direction is CW (forward) More... | |
#define | EQEP_STS_DIR_LATCH (0x0010U) |
Direction was CW on index. More... | |
#define | EQEP_STS_CAP_OVRFLW_ERROR (0x0008U) |
Capture timer overflow. More... | |
#define | EQEP_STS_CAP_DIR_ERROR (0x0004U) |
Direction changed between position capture events. More... | |
#define | EQEP_STS_1ST_IDX_FLAG (0x0002U) |
First index pulse occurred. More... | |
#define | EQEP_STS_POS_CNT_ERROR (0x0001U) |
Position counter error. More... | |
#define | EQEP_LATCH_CNT_READ_BY_CPU (0x0000U) |
On position counter read. More... | |
#define | EQEP_LATCH_UNIT_TIME_OUT (0x0004U) |
On unit time-out event. More... | |
#define | EQEP_LATCH_RISING_STROBE (0x0000U) |
On rising edge of strobe. More... | |
#define | EQEP_LATCH_EDGE_DIR_STROBE (0x0040U) |
On rising edge when clockwise, on falling when counter clockwise. More... | |
#define | EQEP_LATCH_RISING_INDEX (0x0010U) |
On rising edge of index. More... | |
#define | EQEP_LATCH_FALLING_INDEX (0x0020U) |
On falling edge of index. More... | |
#define | EQEP_LATCH_SW_INDEX_MARKER (0x0030U) |
On software index marker. More... | |
#define | EQEP_INIT_DO_NOTHING (0x0000U) |
Action is disabled. More... | |
#define | EQEP_INIT_RISING_STROBE (0x0800U) |
On rising edge of strobe. More... | |
#define | EQEP_INIT_EDGE_DIR_STROBE (0x0C00U) |
On rising edge when clockwise, on falling when counter clockwise. More... | |
#define | EQEP_INIT_RISING_INDEX (0x0200U) |
On rising edge of index. More... | |
#define | EQEP_INIT_FALLING_INDEX (0x0300U) |
On falling edge of index. More... | |
#define EQEP_CONFIG_QUADRATURE (0x0000U) |
Header files.
< Quadrature-clock mode Direction-count mode
#define EQEP_CONFIG_CLOCK_DIR (0x4000U) |
Up-count mode, QDIR = 1.
#define EQEP_CONFIG_UP_COUNT (0x8000U) |
Down-count mode, QDIR = 0.
#define EQEP_CONFIG_DOWN_COUNT (0xC000U) |
#define EQEP_CONFIG_2X_RESOLUTION (0x0000U) |
< Count rising and falling edge
Count rising edge only
#define EQEP_CONFIG_1X_RESOLUTION (0x0800U) |
#define EQEP_CONFIG_NO_SWAP (0x0000U) |
< Do not swap QEPA and QEPB
Swap QEPA and QEPB
#define EQEP_CONFIG_SWAP (0x0400U) |
#define EQEP_COMPARE_NO_SYNC_OUT (0x0000U) |
< Disable sync output
Sync output on index pin
#define EQEP_COMPARE_IDX_SYNC_OUT (0x2000U) |
Sync output on strobe pin.
#define EQEP_COMPARE_STROBE_SYNC_OUT (0x3000U) |
#define EQEP_COMPARE_NO_SHADOW (0x0000U) |
< Disable shadow of QPOSCMP
Load on QPOSCNT = 0
#define EQEP_COMPARE_LOAD_ON_ZERO (0x8000U) |
Load on QPOSCNT = QPOSCMP.
#define EQEP_COMPARE_LOAD_ON_MATCH (0xC000U) |
#define EQEP_INT_GLOBAL (0x0001U) |
Global interrupt flag.
#define EQEP_INT_POS_CNT_ERROR (0x0002U) |
Position counter error.
#define EQEP_INT_PHASE_ERROR (0x0004U) |
Quadrature phase error.
#define EQEP_INT_DIR_CHANGE (0x0008U) |
Quadrature direction change.
#define EQEP_INT_WATCHDOG (0x0010U) |
Watchdog time-out.
#define EQEP_INT_UNDERFLOW (0x0020U) |
Position counter underflow.
#define EQEP_INT_OVERFLOW (0x0040U) |
Position counter overflow.
#define EQEP_INT_POS_COMP_READY (0x0080U) |
Position-compare ready.
#define EQEP_INT_POS_COMP_MATCH (0x0100U) |
Position-compare match.
#define EQEP_INT_STROBE_EVNT_LATCH (0x0200U) |
Strobe event latch.
#define EQEP_INT_INDEX_EVNT_LATCH (0x0400U) |
Index event latch.
#define EQEP_INT_UNIT_TIME_OUT (0x0800U) |
Unit time-out.
#define EQEP_INT_QMA_ERROR (0x1000U) |
QMA error.
#define EQEP_STS_UNIT_POS_EVNT (0x0080U) |
Unit position event detected.
#define EQEP_STS_DIR_ON_1ST_IDX (0x0040U) |
Direction was clockwise on first index event.
#define EQEP_STS_DIR_FLAG (0x0020U) |
Direction is CW (forward)
#define EQEP_STS_DIR_LATCH (0x0010U) |
Direction was CW on index.
#define EQEP_STS_CAP_OVRFLW_ERROR (0x0008U) |
Capture timer overflow.
#define EQEP_STS_CAP_DIR_ERROR (0x0004U) |
Direction changed between position capture events.
#define EQEP_STS_1ST_IDX_FLAG (0x0002U) |
First index pulse occurred.
#define EQEP_STS_POS_CNT_ERROR (0x0001U) |
Position counter error.
#define EQEP_LATCH_CNT_READ_BY_CPU (0x0000U) |
On position counter read.
#define EQEP_LATCH_UNIT_TIME_OUT (0x0004U) |
On unit time-out event.
#define EQEP_LATCH_RISING_STROBE (0x0000U) |
On rising edge of strobe.
#define EQEP_LATCH_EDGE_DIR_STROBE (0x0040U) |
On rising edge when clockwise, on falling when counter clockwise.
#define EQEP_LATCH_RISING_INDEX (0x0010U) |
On rising edge of index.
#define EQEP_LATCH_FALLING_INDEX (0x0020U) |
On falling edge of index.
#define EQEP_LATCH_SW_INDEX_MARKER (0x0030U) |
On software index marker.
#define EQEP_INIT_DO_NOTHING (0x0000U) |
Action is disabled.
#define EQEP_INIT_RISING_STROBE (0x0800U) |
On rising edge of strobe.
#define EQEP_INIT_EDGE_DIR_STROBE (0x0C00U) |
On rising edge when clockwise, on falling when counter clockwise.
#define EQEP_INIT_RISING_INDEX (0x0200U) |
On rising edge of index.
#define EQEP_INIT_FALLING_INDEX (0x0300U) |
On falling edge of index.
Values that can be passed to EQEP_setPositionCounterConfig() as the mode parameter.
enum EQEP_CAPCLKPrescale |
Values that can be passed to EQEP_setCaptureConfig() as the capPrescale parameter. CAPCLK is the capture timer clock frequency.
enum EQEP_UPEVNTPrescale |
Values that can be passed to EQEP_setCaptureConfig() as the evntPrescale parameter. UPEVNT is the unit position event frequency.
enum EQEP_StrobeSource |
Values that can be passed to EQEP_setStrobeSource() as the strobeSrc parameter.
Enumerator | |
---|---|
EQEP_STROBE_FROM_GPIO | Strobe signal comes from GPIO. |
EQEP_STROBE_OR_ADCSOCA | Strobe signal is OR'd with ADCSOCA. |
EQEP_STROBE_OR_ADCSOCB | Strobe signal is OR'd with ADCSOCB. |
enum EQEP_QMAMode |
Values that can be passed to EQEP_setQMAModuleMode() as the qmaMode parameter.
Enumerator | |
---|---|
EQEP_QMA_MODE_BYPASS | QMA module is bypassed. |
EQEP_QMA_MODE_1 | QMA mode-1 operation is selected. |
EQEP_QMA_MODE_2 | QMA mode-2 operation is selected. |
enum EQEP_Source |
Possible values of sources for QEPA,QEPB and Index signal which are passed as a structure to EQEP_selectSource() as sourceConfig
enum EQEP_EmulationMode |
Values that can be passed to EQEP_setEmulationMode() as the emuMode parameter.
Enumerator | |
---|---|
EQEP_EMULATIONMODE_STOPIMMEDIATELY | Counters stop immediately. |
EQEP_EMULATIONMODE_STOPATROLLOVER | Counters stop at period rollover. |
EQEP_EMULATIONMODE_RUNFREE | Counter unaffected by suspend. |
|
inlinestatic |
Enables the eQEP module.
base | is the base address of the eQEP module. |
This function enables operation of the enhanced quadrature encoder pulse (eQEP) module. The module must be configured before it is enabled.
|
inlinestatic |
Disables the eQEP module.
base | is the base address of the enhanced quadrature encoder pulse (eQEP) module |
This function disables operation of the eQEP module.
|
inlinestatic |
Configures eQEP module's quadrature decoder unit.
base | is the base address of the eQEP module. |
config | is the configuration for the eQEP module decoder unit. |
This function configures the operation of the eQEP module's quadrature decoder unit. The config parameter provides the configuration of the decoder and is the logical OR of several values:
|
inlinestatic |
Configures eQEP module position counter unit.
base | is the base address of the eQEP module. |
mode | is the configuration for the eQEP module position counter. |
maxPosition | specifies the maximum position value. |
This function configures the operation of the eQEP module position counter. The mode parameter determines the event on which the position counter gets reset. It should be passed one of the following values: EQEP_POSITION_RESET_IDX, EQEP_POSITION_RESET_MAX_POS, EQEP_POSITION_RESET_1ST_IDX, or EQEP_POSITION_RESET_UNIT_TIME_OUT.
maxPosition is the maximum value of the position counter and is the value used to reset the position capture when moving in the reverse (negative) direction.
|
inlinestatic |
Gets the current encoder position.
base | is the base address of the eQEP module. |
This function returns the current position of the encoder. Depending upon the configuration of the encoder, and the incident of an index pulse, this value may or may not contain the expected data (that is, if in reset on index mode, if an index pulse has not been encountered, the position counter is not yet aligned with the index pulse).
|
inlinestatic |
Sets the current encoder position.
base | is the base address of the eQEP module. |
position | is the new position for the encoder. |
This function sets the current position of the encoder; the encoder position is then measured relative to this value.
|
inlinestatic |
Gets the current direction of rotation.
base | is the base address of the eQEP module. |
This function returns the current direction of rotation. In this case, current means the most recently detected direction of the encoder; it may not be presently moving but this is the direction it last moved before it stopped.
|
inlinestatic |
Enables individual eQEP module interrupt sources.
base | is the base address of the eQEP module. |
intFlags | is a bit mask of the interrupt sources to be enabled. |
This function enables eQEP module interrupt sources. The intFlags parameter can be any of the following values OR'd together:
|
inlinestatic |
Disables individual eQEP module interrupt sources.
base | is the base address of the eQEP module. |
intFlags | is a bit mask of the interrupt sources to be disabled. |
This function disables eQEP module interrupt sources. The intFlags parameter can be any of the following values OR'd together:
|
inlinestatic |
Gets the current interrupt status.
base | is the base address of the eQEP module. |
This function returns the interrupt status for the eQEP module module.
|
inlinestatic |
Clears eQEP module interrupt sources.
base | is the base address of the eQEP module. |
intFlags | is a bit mask of the interrupt sources to be cleared. |
This function clears eQEP module interrupt flags. The intFlags parameter can be any of the following values OR'd together:
Note that the EQEP_INT_GLOBAL value is the global interrupt flag. In order to get any further eQEP interrupts, this flag must be cleared.
|
inlinestatic |
Forces individual eQEP module interrupts.
base | is the base address of the eQEP module. |
intFlags | is a bit mask of the interrupt sources to be forced. |
This function forces eQEP module interrupt flags. The intFlags parameter can be any of the following values OR'd together:
|
inlinestatic |
Gets the encoder error indicator.
base | is the base address of the eQEP module. |
This function returns the error indicator for the eQEP module. It is an error for both of the signals of the quadrature input to change at the same time.
|
inlinestatic |
Returns content of the eQEP module status register
base | is the base address of the eQEP module. |
This function returns the contents of the status register. The value it returns is an OR of the following values:
|
inlinestatic |
Clears selected fields of the eQEP module status register
base | is the base address of the eQEP module. |
statusFlags | is the bit mask of the status flags to be cleared. |
This function clears the status register fields indicated by statusFlags. The statusFlags parameter is the logical OR of any of the following:
|
inlinestatic |
Configures eQEP module edge-capture unit.
base | is the base address of the eQEP module. |
capPrescale | is the prescaler setting of the eQEP capture timer clk. |
evntPrescale | is the prescaler setting of the unit position event frequency. |
This function configures the operation of the eQEP module edge-capture unit. The capPrescale parameter provides the configuration of the eQEP capture timer clock rate. It determines by which power of 2 between 1 and 128 inclusive SYSCLKOUT is divided. The macros for this parameter are in the format of EQEP_CAPTURE_CLK_DIV_X, where X is the divide value. For example, EQEP_CAPTURE_CLK_DIV_32 will give a capture timer clock frequency that is SYSCLKOUT/32.
The evntPrescale parameter determines how frequently a unit position event occurs. The macro that can be passed this parameter is in the format EQEP_UNIT_POS_EVNT_DIV_X, where X is the number of quadrature clock periods between unit position events. For example, EQEP_UNIT_POS_EVNT_DIV_16 will result in a unit position event frequency of QCLK/16.
|
inlinestatic |
Enables the eQEP module edge-capture unit.
base | is the base address of the eQEP module. |
This function enables operation of the eQEP module's edge-capture unit.
|
inlinestatic |
Disables the eQEP module edge-capture unit.
base | is the base address of the eQEP module. |
This function disables operation of the eQEP module's edge-capture unit.
|
inlinestatic |
Gets the encoder capture period.
base | is the base address of the eQEP module. |
This function returns the period count value between the last successive eQEP position events.
|
inlinestatic |
Gets the encoder capture timer value.
base | is the base address of the eQEP module. |
This function returns the time base for the edge capture unit.
|
inlinestatic |
Enables the eQEP module position-compare unit.
base | is the base address of the eQEP module. |
This function enables operation of the eQEP module's position-compare unit.
|
inlinestatic |
Disables the eQEP module position-compare unit.
base | is the base address of the eQEP module. |
This function disables operation of the eQEP module's position-compare unit.
|
inlinestatic |
Configures the position-compare unit's sync output pulse width.
base | is the base address of the eQEP module. |
cycles | is the width of the pulse that can be generated on a position-compare event. It is in units of 4 SYSCLKOUT cycles. |
This function configures the width of the sync output pulse. The width of the pulse will be cycles * 4 * the width of a SYSCLKOUT cycle. The maximum width is 4096 * 4 * SYSCLKOUT cycles.
|
inlinestatic |
Loads the eQEP module unit timer period as number of SYSCLK cycles.
base | is the base address of the eQEP module. |
period | is period value at which a unit time-out interrupt is set. |
This function sets the unit time-out interrupt when it matches the value specified by period The unit timer is clocked by SYSCLKOUT
|
inlinestatic |
Enables the eQEP module unit timer.
base | is the base address of the eQEP module. |
period | is period value at which a unit time-out interrupt is set. |
This function enables operation of the eQEP module's peripheral unit timer. The unit timer is clocked by SYSCLKOUT and will set the unit time-out interrupt when it matches the value specified by period.
|
inlinestatic |
Disables the eQEP module unit timer.
base | is the base address of the eQEP module. |
This function disables operation of the eQEP module's peripheral unit timer.
|
inlinestatic |
Enables the eQEP module watchdog timer.
base | is the base address of the eQEP module. |
period | is watchdog period value at which a time-out will occur if no quadrature-clock event is detected. |
This function enables operation of the eQEP module's peripheral watchdog timer.
|
inlinestatic |
Disables the eQEP module watchdog timer.
base | is the base address of the eQEP module. |
This function disables operation of the eQEP module's peripheral watchdog timer.
|
inlinestatic |
Sets the eQEP module watchdog timer value.
base | is the base address of the eQEP module. |
value | is the value to be written to the watchdog timer. |
This function sets the eQEP module's watchdog timer value.
|
inlinestatic |
Gets the eQEP module watchdog timer value.
base | is the base address of the eQEP module. |
|
inlinestatic |
Configures the mode in which the position counter is initialized.
base | is the base address of the eQEP module. |
initMode | is the configuration for initializing the position count. See below for a description of this parameter. |
This function configures the events on which the position count can be initialized. The initMode parameter provides the mode as either EQEP_INIT_DO_NOTHING (no action configured) or one of the following strobe events, index events, or a logical OR of both a strobe event and an index event.
Use EQEP_setSWPositionInit() to cause a software initialization and EQEP_setInitialPosition() to set the value that gets loaded into the position counter upon initialization.
|
inlinestatic |
Sets the software initialization of the encoder position counter.
base | is the base address of the eQEP module. |
initialize | is a flag to specify if software initialization of the position counter is enabled. |
This function does a software initialization of the position counter when the initialize parameter is true. When false, the QEPCTL[SWI] bit is cleared and no action is taken.
The init value to be loaded into the position counter can be set with EQEP_setInitialPosition(). Additional initialization causes can be configured with EQEP_setPositionInitMode().
|
inlinestatic |
Sets the init value for the encoder position counter.
base | is the base address of the eQEP module. |
position | is the value to be written to the position counter upon. initialization. |
This function sets the init value for position of the encoder. See EQEP_setPositionInitMode() to set the initialization cause or EQEP_setSWPositionInit() to cause a software initialization.
|
inlinestatic |
Configures the quadrature modes in which the position count can be latched.
base | is the base address of the eQEP module. |
latchMode | is the configuration for latching of the position count and several other registers. See below for a description of this parameter. |
This function configures the events on which the position count and several other registers can be latched. The latchMode parameter provides the mode as the logical OR of several values.
|
inlinestatic |
Gets the encoder position that was latched on an index event.
base | is the base address of the eQEP module. |
This function returns the value in the index position latch register. The position counter is latched into this register on either a rising index edge, a falling index edge, or a software index marker. This is configured using EQEP_setLatchMode().
|
inlinestatic |
Gets the encoder position that was latched on a strobe event.
base | is the base address of the eQEP module. |
This function returns the value in the strobe position latch register. The position counter can be configured to be latched into this register on rising strobe edges only or on rising strobe edges while moving clockwise and falling strobe edges while moving counter-clockwise. This is configured using EQEP_setLatchMode().
|
inlinestatic |
Gets the encoder position that was latched on a unit time-out event.
base | is the base address of the eQEP module. |
This function returns the value in the position latch register. The position counter is latched into this register either on a unit time-out event.
|
inlinestatic |
Gets the encoder capture timer latch.
base | is the base address of the eQEP module. |
This function returns the value in the capture timer latch register. The capture timer value is latched into this register either on a unit time-out event or upon the CPU reading the eQEP position counter. This is configured using EQEP_setLatchMode().
|
inlinestatic |
Gets the encoder capture period latch.
base | is the base address of the eQEP module. |
This function returns the value in the capture period latch register. The capture period value is latched into this register either on a unit time-out event or upon the CPU reading the eQEP position counter. This is configured using EQEP_setLatchMode().
|
inlinestatic |
Set the quadrature mode adapter (QMA) module mode
base | is the base address of the eQEP module. |
qmaMode | is the mode in which the QMA module will operate. |
This function sets the quadrature mode adapter module mode. The possible modes are passed to the function through the qmaMode parameter which can take the values EQEP_QMA_MODE_BYPASS, EQEP_QMA_MODE_1, or EQEP_QMA_MODE_2.
To use the QMA module, you must first put the eQEP module into direction-count mode ( EQEP_CONFIG_CLOCK_DIR) using EQEP_setConfig().
|
inlinestatic |
Set the strobe input source of the eQEP module.
base | is the base address of the eQEP module. |
strobeSrc | is the source of the strobe signal. |
This function sets the source of the eQEP module's strobe signal. The possible values of the strobeSrc parameter are
|
inlinestatic |
Enables the index direction enhancement mode of the eQEP module
base | is the base address of the eQEP module. |
This function enables the enhancement mode for direction change during Index event
|
inlinestatic |
Disables the index direction enhancement mode of the eQEP module
base | is the base address of the eQEP module. |
This function disables the enhancement mode for direction change during Index event
|
inlinestatic |
Selects the source for eQEPA/B/I signals
base | is the base address of the enhanced quadrature encoder pulse (eQEP) module |
sourceConfig | is the structure that contains source configuration |
This function configures the sources for QEPA,QEPB and Index of eQEP module
|
inlinestatic |
Set the emulation mode of the eQEP module.
base | is the base address of the eQEP module. |
emuMode | is the mode operation upon an emulation suspend. |
This function sets the eQEP module's emulation mode. This mode determines how the timers are affected by an emulation suspend. Valid values for the emuMode parameter are the following:
void EQEP_setCompareConfig | ( | uint32_t | base, |
uint16_t | config, | ||
uint32_t | compareValue, | ||
uint16_t | cycles | ||
) |
Configures eQEP module position-compare unit.
base | is the base address of the eQEP module. |
config | is the configuration for the eQEP module position-compare unit. See below for a description of this parameter. |
compareValue | is the value to which the position count value is compared for a position-compare event. |
cycles | is the width of the pulse that can be generated on a position-compare event. It is in units of 4 SYSCLKOUT cycles. |
This function configures the operation of the eQEP module position-compare unit. The config parameter provides the configuration of the position-compare unit and is the logical OR of several values:
The cycles is used to select the width of the sync output pulse. The width of the resulting pulse will be cycles * 4 * the width of a SYSCLKOUT cycle. The maximum width is 4096 * 4 * SYSCLKOUT cycles.
void EQEP_setInputPolarity | ( | uint32_t | base, |
bool | invertQEPA, | ||
bool | invertQEPB, | ||
bool | invertIndex, | ||
bool | invertStrobe | ||
) |
Sets the polarity of the eQEP module's input signals.
base | is the base address of the eQEP module. |
invertQEPA | is the flag to negate the QEPA input. |
invertQEPB | is the flag to negate the QEPA input. |
invertIndex | is the flag to negate the index input. |
invertStrobe | is the flag to negate the strobe input. |
This function configures the polarity of the inputs to the eQEP module. To negate the polarity of any of the input signals, pass true into its corresponding parameter in this function. Pass false to leave it as-is.