AM263Px MCU+ SDK  11.01.00

Detailed Description

Parameters passed during PMIC_open()

Forward declaration of PMIC_Params_s.

Data Fields

uint32_t deviceType
 
uint32_t commMode
 
uint32_t instType
 
uint32_t i2cAddr
 
uint32_t instance
 

Field Documentation

◆ deviceType

uint32_t PMIC_Params::deviceType

PMIC device type

◆ commMode

uint32_t PMIC_Params::commMode

PMIC Interface mode - Single I2C, Dual I2C or SPI.

◆ instType

uint32_t PMIC_Params::instType

PMIC Instance type.

◆ i2cAddr

uint32_t PMIC_Params::i2cAddr

Underlying I2C peripheral device address that is used by the PMIC driver

◆ instance

uint32_t PMIC_Params::instance

Underlying I2C/MCSPI peripheral driver instance that is used by the PMIC driver