AM263Px MCU+ SDK  11.01.00
OSPI_ReadCmdParams Struct Reference

Detailed Description

OSPI Instance Read Command Structure.

Data Fields

uint8_t cmd
 
uint32_t cmdAddr
 
uint8_t numAddrBytes
 
uint8_t dummyBits
 
void * rxDataBuf
 
uint16_t rxDataLen
 
uint32_t readTimeout
 

Field Documentation

◆ cmd

uint8_t OSPI_ReadCmdParams::cmd

[IN] Command Opcode

◆ cmdAddr

uint32_t OSPI_ReadCmdParams::cmdAddr

Address required by the command. Usually needed in reading flash registers. Should be initialized to OSPI_CMD_INVALID_ADDR if not used.

◆ numAddrBytes

uint8_t OSPI_ReadCmdParams::numAddrBytes

[IN] Number of address bytes used to send cmd address

◆ dummyBits

uint8_t OSPI_ReadCmdParams::dummyBits

[IN] Number dummyClks needed for the command

◆ rxDataBuf

void* OSPI_ReadCmdParams::rxDataBuf

[OUT] Buffer to store response from flash

◆ rxDataLen

uint16_t OSPI_ReadCmdParams::rxDataLen

[IN] Length of response buffer

◆ readTimeout

uint32_t OSPI_ReadCmdParams::readTimeout

[IN] Timeout of the specific read