AM263Px MCU+ SDK  11.01.00
OSPI_PhyWindowParams Struct Reference

Detailed Description

OSPI PHY Tuning Window Parameters.

These are input window parameters for OSPI PHY tuning algorithm. This data is usually SOC specific and is filled by SysConfig.

Data Fields

int32_t txDllLowWindowStart
 
int32_t txDllLowWindowEnd
 
int32_t txDllHighWindowStart
 
int32_t txDllHighWindowEnd
 
int32_t rxLowSearchStart
 
int32_t rxLowSearchEnd
 
int32_t rxHighSearchStart
 
int32_t rxHighSearchEnd
 
int32_t txLowSearchStart
 
int32_t txLowSearchEnd
 
int32_t txHighSearchStart
 
int32_t txHighSearchEnd
 
int32_t txDLLSearchOffset
 
uint32_t rxTxDLLSearchStep
 
uint32_t rdDelayMin
 
uint32_t rdDelayMax
 

Field Documentation

◆ txDllLowWindowStart

int32_t OSPI_PhyWindowParams::txDllLowWindowStart

◆ txDllLowWindowEnd

int32_t OSPI_PhyWindowParams::txDllLowWindowEnd

◆ txDllHighWindowStart

int32_t OSPI_PhyWindowParams::txDllHighWindowStart

◆ txDllHighWindowEnd

int32_t OSPI_PhyWindowParams::txDllHighWindowEnd

◆ rxLowSearchStart

int32_t OSPI_PhyWindowParams::rxLowSearchStart

◆ rxLowSearchEnd

int32_t OSPI_PhyWindowParams::rxLowSearchEnd

◆ rxHighSearchStart

int32_t OSPI_PhyWindowParams::rxHighSearchStart

◆ rxHighSearchEnd

int32_t OSPI_PhyWindowParams::rxHighSearchEnd

◆ txLowSearchStart

int32_t OSPI_PhyWindowParams::txLowSearchStart

◆ txLowSearchEnd

int32_t OSPI_PhyWindowParams::txLowSearchEnd

◆ txHighSearchStart

int32_t OSPI_PhyWindowParams::txHighSearchStart

◆ txHighSearchEnd

int32_t OSPI_PhyWindowParams::txHighSearchEnd

◆ txDLLSearchOffset

int32_t OSPI_PhyWindowParams::txDLLSearchOffset

◆ rxTxDLLSearchStep

uint32_t OSPI_PhyWindowParams::rxTxDLLSearchStep

◆ rdDelayMin

uint32_t OSPI_PhyWindowParams::rdDelayMin

◆ rdDelayMax

uint32_t OSPI_PhyWindowParams::rdDelayMax