AM263Px MCU+ SDK  11.01.00

Detailed Description

MMCSD instance attributes - used during init time.

Data Fields

uint32_t baseAddr
 
uint32_t inputClk
 
bool enableDma
 
bool intrEnable
 
uint32_t intrPriority
 
uint32_t intrNum
 
uint32_t eventId
 
uint32_t cardType
 
uint32_t busWidth
 
bool autoAssignMaxSpeed
 
uint32_t uaBusSpeed
 

Field Documentation

◆ baseAddr

uint32_t MMCSD_Attrs::baseAddr

MMCSD subsystem registers base address

◆ inputClk

uint32_t MMCSD_Attrs::inputClk

MMC input functional clock

◆ enableDma

bool MMCSD_Attrs::enableDma

DMA Enable

◆ intrEnable

bool MMCSD_Attrs::intrEnable

Module interrupt enable

◆ intrPriority

uint32_t MMCSD_Attrs::intrPriority

Priority of interrupt for MMCSD ISR

◆ intrNum

uint32_t MMCSD_Attrs::intrNum

Module interrupt vector

◆ eventId

uint32_t MMCSD_Attrs::eventId

Module interrupt event ID

◆ cardType

uint32_t MMCSD_Attrs::cardType

Type of card

◆ busWidth

uint32_t MMCSD_Attrs::busWidth

Supported bus width

◆ autoAssignMaxSpeed

bool MMCSD_Attrs::autoAssignMaxSpeed

Auto Assign Maximum Speed

◆ uaBusSpeed

uint32_t MMCSD_Attrs::uaBusSpeed

User Assigned Bus Speed Mode