AM263Px MCU+ SDK  11.01.00
ICSS_EMAC_PruStatistics Struct Reference

Detailed Description

Statistics structure for capturing statistics on PRU.

Data Fields

volatile uint32_t txBcast
 
volatile uint32_t txMcast
 
volatile uint32_t txUcast
 
volatile uint32_t txOctets
 
volatile uint32_t rxBcast
 
volatile uint32_t rxMcast
 
volatile uint32_t rxUcast
 
volatile uint32_t rxOctets
 
volatile uint32_t tx64byte
 
volatile uint32_t tx65_127byte
 
volatile uint32_t tx128_255byte
 
volatile uint32_t tx256_511byte
 
volatile uint32_t tx512_1023byte
 
volatile uint32_t tx1024byte
 
volatile uint32_t rx64byte
 
volatile uint32_t rx65_127byte
 
volatile uint32_t rx128_255byte
 
volatile uint32_t rx256_511byte
 
volatile uint32_t rx512_1023byte
 
volatile uint32_t rx1024byte
 
volatile uint32_t lateColl
 
volatile uint32_t singleColl
 
volatile uint32_t multiColl
 
volatile uint32_t excessColl
 
volatile uint32_t rxMisAlignmentFrames
 
volatile uint32_t stormPrevCounter
 
volatile uint32_t stormPrevCounterMC
 
volatile uint32_t stormPrevCounterUC
 
volatile uint32_t macRxError
 
volatile uint32_t SFDError
 
volatile uint32_t defTx
 
volatile uint32_t macTxError
 
volatile uint32_t rxOverSizedFrames
 
volatile uint32_t rxUnderSizedFrames
 
volatile uint32_t rxCRCFrames
 
volatile uint32_t droppedPackets
 
volatile uint32_t txOverFlow
 
volatile uint32_t txUnderFlow
 
volatile uint32_t sqeTestError
 
volatile uint32_t TXqueueLevel
 
volatile uint32_t CSError
 

Field Documentation

◆ txBcast

volatile uint32_t ICSS_EMAC_PruStatistics::txBcast

◆ txMcast

volatile uint32_t ICSS_EMAC_PruStatistics::txMcast

Number of broadcast packets sent

◆ txUcast

volatile uint32_t ICSS_EMAC_PruStatistics::txUcast

Number of multicast packets sent

◆ txOctets

volatile uint32_t ICSS_EMAC_PruStatistics::txOctets

Number of unicast packets sent

◆ rxBcast

volatile uint32_t ICSS_EMAC_PruStatistics::rxBcast

Number of Tx packets

◆ rxMcast

volatile uint32_t ICSS_EMAC_PruStatistics::rxMcast

Number of broadcast packets rcvd

◆ rxUcast

volatile uint32_t ICSS_EMAC_PruStatistics::rxUcast

Number of multicast packets rcvd

◆ rxOctets

volatile uint32_t ICSS_EMAC_PruStatistics::rxOctets

Number of unicast packets rcvd

◆ tx64byte

volatile uint32_t ICSS_EMAC_PruStatistics::tx64byte

Number of Rx packets

◆ tx65_127byte

volatile uint32_t ICSS_EMAC_PruStatistics::tx65_127byte

Number of 64 byte packets sent

◆ tx128_255byte

volatile uint32_t ICSS_EMAC_PruStatistics::tx128_255byte

Number of 65-127 byte packets sent

◆ tx256_511byte

volatile uint32_t ICSS_EMAC_PruStatistics::tx256_511byte

Number of 128-255 byte packets sent

◆ tx512_1023byte

volatile uint32_t ICSS_EMAC_PruStatistics::tx512_1023byte

Number of 256-511 byte packets sent

◆ tx1024byte

volatile uint32_t ICSS_EMAC_PruStatistics::tx1024byte

Number of 512-1023 byte packets sent

◆ rx64byte

volatile uint32_t ICSS_EMAC_PruStatistics::rx64byte

Number of 1024 and larger size packets sent

◆ rx65_127byte

volatile uint32_t ICSS_EMAC_PruStatistics::rx65_127byte

Number of 64 byte packets rcvd

◆ rx128_255byte

volatile uint32_t ICSS_EMAC_PruStatistics::rx128_255byte

Number of 65-127 byte packets rcvd

◆ rx256_511byte

volatile uint32_t ICSS_EMAC_PruStatistics::rx256_511byte

Number of 128-255 byte packets rcvd

◆ rx512_1023byte

volatile uint32_t ICSS_EMAC_PruStatistics::rx512_1023byte

Number of 256-511 byte packets rcvd

◆ rx1024byte

volatile uint32_t ICSS_EMAC_PruStatistics::rx1024byte

Number of 512-1023 byte packets rcvd

◆ lateColl

volatile uint32_t ICSS_EMAC_PruStatistics::lateColl

Number of 1024 and larger size packets rcvd

◆ singleColl

volatile uint32_t ICSS_EMAC_PruStatistics::singleColl

Number of late collisions(Half Duplex)

◆ multiColl

volatile uint32_t ICSS_EMAC_PruStatistics::multiColl

Number of single collisions (Half Duplex)

◆ excessColl

volatile uint32_t ICSS_EMAC_PruStatistics::excessColl

Number of multiple collisions (Half Duplex)

◆ rxMisAlignmentFrames

volatile uint32_t ICSS_EMAC_PruStatistics::rxMisAlignmentFrames

Number of excess collisions(Half Duplex)

◆ stormPrevCounter

volatile uint32_t ICSS_EMAC_PruStatistics::stormPrevCounter

Number of non multiple of 8 byte frames rcvd

◆ stormPrevCounterMC

volatile uint32_t ICSS_EMAC_PruStatistics::stormPrevCounterMC

Number of packets dropped because of Storm Prevention (broadcast)

◆ stormPrevCounterUC

volatile uint32_t ICSS_EMAC_PruStatistics::stormPrevCounterUC

Number of packets dropped because of Storm Prevention (multicast)

◆ macRxError

volatile uint32_t ICSS_EMAC_PruStatistics::macRxError

Number of packets dropped because of Storm Prevention (unicast)

◆ SFDError

volatile uint32_t ICSS_EMAC_PruStatistics::SFDError

Number of MAC receive errors

◆ defTx

volatile uint32_t ICSS_EMAC_PruStatistics::defTx

Number of invalid SFD

◆ macTxError

volatile uint32_t ICSS_EMAC_PruStatistics::macTxError

Number of transmissions deferred

◆ rxOverSizedFrames

volatile uint32_t ICSS_EMAC_PruStatistics::rxOverSizedFrames

Number of MAC transmit errors

◆ rxUnderSizedFrames

volatile uint32_t ICSS_EMAC_PruStatistics::rxUnderSizedFrames

Number of oversized frames rcvd

◆ rxCRCFrames

volatile uint32_t ICSS_EMAC_PruStatistics::rxCRCFrames

Number of undersized frames rcvd

◆ droppedPackets

volatile uint32_t ICSS_EMAC_PruStatistics::droppedPackets

Number of CRC error frames rcvd

◆ txOverFlow

volatile uint32_t ICSS_EMAC_PruStatistics::txOverFlow

Number of packets dropped due to a link down on opposite port

◆ txUnderFlow

volatile uint32_t ICSS_EMAC_PruStatistics::txUnderFlow

Tx FIFO overflow count

◆ sqeTestError

volatile uint32_t ICSS_EMAC_PruStatistics::sqeTestError

Tx FIFO underflow count

◆ TXqueueLevel

volatile uint32_t ICSS_EMAC_PruStatistics::TXqueueLevel

Number of MAC receive errors

◆ CSError

volatile uint32_t ICSS_EMAC_PruStatistics::CSError

Current Tx queue level