AM263Px MCU+ SDK  26.00.00
sipc_notify_src.h File Reference

Go to the source code of this file.

Data Structures

struct  SIPC_InterruptConfig
 This structure describes the information related to one interrupt that is setup for receiving mailbox messages One interrupt can be used to handle messages from multiple cores. More...
 
struct  SIPC_MailboxConfig
 This structure describes the mailbox information to send a message from core A to core B. More...
 

Functions

int32_t SIPC_Register_Isr (HwiP_Params *pHwiParams, SIPC_InterruptConfig *pInterruptConfig, SIPC_Params *params, HwiP_FxnCallback callback)
 Register SIPC interrupts for SOC. More...
 
void SIPC_isr (void *args)
 

Variables

SIPC_MailboxConfig gSIPC_SecureHostMboxConfig [CORE_ID_MAX - 1U]
 Global structure that is pre-defined for this SOC to configure any R5 CPU to HSM mailbox communication. More...
 
SIPC_MailboxConfig gSIPC_HsmMboxConfig [CORE_ID_MAX - 1U]
 Global structure that is pre-defined for this SOC to configure any R5 CPU to HSM mailbox communication. More...
 
SIPC_SwQueue * gSIPC_QueSecureHostToHsm [MAX_SEC_CORES_WITH_HSM - 1U]
 Global structure holding R5 to HSM queues addresses indexed by sec core id. More...
 
SIPC_SwQueue * gSIPC_QueHsmToSecureHost [MAX_SEC_CORES_WITH_HSM - 1U]
 Global structure holding HSM -> R5 queues addresses indexed by sec core id. More...
 

Function Documentation

◆ SIPC_Register_Isr()

int32_t SIPC_Register_Isr ( HwiP_Params *  pHwiParams,
SIPC_InterruptConfig *  pInterruptConfig,
SIPC_Params *  params,
HwiP_FxnCallback  callback 
)

Register SIPC interrupts for SOC.

This API will register SIPC interrupts. This API acts as an abstraction layer to register interrupts for different SOCs having different interrupt controllers

◆ SIPC_isr()

void SIPC_isr ( void *  args)

Variable Documentation

◆ gSIPC_SecureHostMboxConfig

SIPC_MailboxConfig gSIPC_SecureHostMboxConfig[CORE_ID_MAX - 1U]
extern

Global structure that is pre-defined for this SOC to configure any R5 CPU to HSM mailbox communication.

This is a pre-defined global since this config typically does not need to change based on end user use-cases for this SOC.

◆ gSIPC_HsmMboxConfig

SIPC_MailboxConfig gSIPC_HsmMboxConfig[CORE_ID_MAX - 1U]
extern

Global structure that is pre-defined for this SOC to configure any R5 CPU to HSM mailbox communication.

This is a pre-defined global since this config typically does not need to change based on end user use-cases for this SOC.

◆ gSIPC_QueSecureHostToHsm

SIPC_SwQueue* gSIPC_QueSecureHostToHsm[MAX_SEC_CORES_WITH_HSM - 1U]
extern

Global structure holding R5 to HSM queues addresses indexed by sec core id.

This is a pre-defined global since this config typically does not need to change based on end user use-cases for this SOC.

◆ gSIPC_QueHsmToSecureHost

SIPC_SwQueue* gSIPC_QueHsmToSecureHost[MAX_SEC_CORES_WITH_HSM - 1U]
extern

Global structure holding HSM -> R5 queues addresses indexed by sec core id.

This is a pre-defined global since this config typically does not need to change based on end user use-cases for this SOC.