AM263Px MCU+ SDK  11.01.00

Introduction

FOTA Agent Driver API/interface file.

Go to the source code of this file.

Data Structures

struct  FOTAAgent_Params
 FOTA Agent Driver Handle. More...
 
struct  FOTAAgent_Handle
 

Macros

#define FOTAAGENT_WRITEOFFSET_DNC   (0U)
 

Functions

int32_t FOTAAgent_Params_init (FOTAAgent_Params *params)
 Initilize params with default values. More...
 
int32_t FOTAAgent_init (FOTAAgent_Handle *pHandle, FOTAAgent_Params *params)
 Initilize FOTA Agent API. More...
 
int32_t FOTAAgent_writeStart (FOTAAgent_Handle *pHandle, uint32_t wrOffset, char doFlashSegments)
 Logically start writes and initilize state internal machine. More...
 
int32_t FOTAAgent_writeUpdate (FOTAAgent_Handle *pHandle, uint8_t *buf, uint32_t size)
 Update internal machine with new data. More...
 
int32_t FOTAAgent_writeEnd (FOTAAgent_Handle *pHandle)
 Logically end writes and end the state machine. More...
 
int32_t FOTAAgent_getFLSOPSKDHandle (FOTAAgent_Handle *pHandle, FLSOPSKD_Handle *flsopskdHandle)
 Retrive FLSOPSKD handle. More...