AM263Px MCU+ SDK  11.01.00
cb_lld_ethernet.h File Reference

Introduction

TI ENET LLD specific network layer part.

Go to the source code of this file.

Data Structures

struct  lld_ethhdr
 Ethernet header structure. More...
 
struct  lld_sockaddr
 Structure representing the lld_sockaddr instance. More...
 
struct  lld_ethdev_t
 Structure representing the lld_ethdev instance. More...
 
struct  cb_socket_lldcfg_update_t
 Structure representing the cb_socket_lldcfg_update instance. More...
 
struct  cb_tilld_port_stats_t
 

Macros

#define LWIP_DONT_PROVIDE_BYTEORDER_FUNCTIONS
 
#define htons   __htons
 
#define ntohs   __ntohs
 
#define htonl   __htonl
 
#define ntohl   __ntohl
 
#define MAX_NUMBER_ENET_DEVS   LLDENET_MAX_PORTS
 
#define CB_SOCKET_VALID(x)   ((x)!=NULL)
 
#define CB_SOCKET_INVALID_VALUE   NULL
 
#define CB_SOCKET_T   lld_socket_t*
 
#define CB_ETHHDR_T   struct lld_ethhdr
 
#define CB_SOCKADDR_LL_T   struct lld_sockaddr
 
#define CB_SOCKADDR_T   struct lld_sockaddr
 
#define CB_SOCK_SENDTO   cb_lld_sendto
 
#define CB_SOCK_CLOSE   cb_rawsock_close
 
#define CB_OPEN   open
 
#define CB_CLOSE   close
 
#define CB_WRITE   write
 
#define CB_IN_ADDR_T   void*
 
#define IFNAMSIZ   16
 
#define ETH_ALEN   6 /* Octets in one ethernet addr */
 
#define ETH_HLEN   14 /* Total octets in header. */
 
#define ETH_DATA_LEN   1500 /* Max. octets in payload */
 
#define ETH_P_8021Q   0x8100 /* 802.1Q VLAN Extended Header */
 
#define ETH_P_1588   0x88F7 /* IEEE 1588 Timesync */
 
#define ETH_P_LLDP   0x88CC /* 802.1AB LLDP */
 
#define ETH_P_TSN   0x22F0 /* TSN (IEEE 1722) packet */
 
#define ETH_P_NETLINK   0x22F1 /* A virtual prototol for netlink rawsockt on TI platforms */
 
#define CB_MAX_NETDEVNAME   16
 
#define MKPIPE(x)   (-1)
 
#define CB_LLD_MAX_ETH_FRAME_SIZE   (1522U)
 
#define CB_TILLD_STATS_BLOCK_ELEM_NUM   (128U)
 

Typedefs

typedef struct lld_socket lld_socket_t
 Structure representing the lld_socket instance. More...
 
typedef int(* cb_socket_lldcfg_update_cb_t) (cb_socket_lldcfg_update_t *update_cfg)
 Callback function type for cb_socket_lldcfg_update. More...
 

Functions

struct lld_ethhdr __attribute__ ((packed))
 
int cb_lld_init_devs_table (lld_ethdev_t *ethdevs, uint32_t ndevs, uint32_t enet_type, uint32_t instance_id, const LLDTsyncTsSource tsSource)
 Initialize a LLD device table. More...
 
int cb_socket_set_lldcfg_update_cb (cb_socket_lldcfg_update_cb_t lldcfg_update_cb)
 This function sets the callback for updating LLD config parameters. It enables the user to update config parameters for the Enet LLD layer that are not supported by the CB socket. It is important to note that this function should only be called once. More...
 
int cb_lld_netdev_to_macport (const char *netdev)
 Convert net device name to mac port. More...
 
int cb_lld_sendto (CB_SOCKET_T sfd, void *sdata, int psize, int flags, const CB_SOCKADDR_LL_T *addr, int addrsize)
 Send a TX ethernet L2 packet. More...
 
int cb_lld_sendto_scatter (CB_SOCKET_T sfd, LLDEnetFrameScatter_t *frame, const CB_SOCKADDR_LL_T *addr)
 Send a TX ethernet L2 packet in the scatter way. More...
 
int cb_lld_recv (CB_SOCKET_T sfd, void *buf, int size, CB_SOCKADDR_LL_T *addr, int addrsize)
 Receive a RX ethernet L2 packet. This should be called after a rxnotify_cb is invoked. More...
 
int cb_lld_recv_zerocopy (CB_SOCKET_T sfd, LLDEnetRecvCb_t cblld_recv_cb, void *cbarg)
 Receive a RX ethernet L2 packet n the zero-copy way. This should be called after a rxnotify_cb is invoked. More...
 
int cb_lld_set_txnotify_cb (CB_SOCKET_T sfd, void(*txnotify_cb)(void *arg), void *arg)
 Set the TX notify callback that is invoked when an TX packet is sent successfully. More...
 
int cb_lld_set_rxnotify_cb (CB_SOCKET_T sfd, void(*rxnotify_cb)(void *arg), void *arg)
 Set the RX notify callback that is invoked when an RX packet is ready to be received. More...
 
int cb_lld_set_default_rxdata_cb (CB_SOCKET_T sfd, void(*default_rxdata_cb)(void *data, int size, int port, void *arg), void *arg)
 Set the default RX data callback that is invoked when an RX packet does not match any filters. More...
 
int cb_lld_get_type_instance (uint32_t *enet_type, uint32_t *instance_id)
 Get enet type and instance that is set via cb_lld_init_devs_table() More...
 
int cb_lld_get_ts_source (LLDTsyncTsSource *tsSource)
 Get Timestamp source that is set via cb_lld_init_devs_table() More...
 
int cb_lld_get_netdevs (char *netdevs[], int *len)
 Get all virtual network interfaces which were defined for the TI platform. More...
 
int cb_lld_get_link_state (CB_SOCKET_T cfd, const char *dev, uint32_t *linkstate)
 get link state from device name like 'eth0' More...
 
int cb_lld_get_link_info (CB_SOCKET_T cfd, const char *dev, uint32_t *speed, uint32_t *duplex)
 get link info(speed and duplex) from device name like 'eth0' More...
 
int cb_lld_get_port_stats (CB_SOCKET_T sfd, int port, cb_tilld_port_stats_t *stats)
 Get stats info from host or mac port. More...
 
void cb_lld_reset_port_stats (CB_SOCKET_T sfd, int port)
 reset stats info from host or mac port. More...
 
int cb_lld_process_status_frames (CB_SOCKET_T sfd)
 process the Phy status frames. More...
 
void cb_lld_notify_linkchange (void)
 Nofity link change event through cbl_query_thread_data_t signal. More...
 

Variables

uint8_t h_dest [ETH_ALEN]
 
uint8_t h_source [ETH_ALEN]
 
uint16_t h_proto
 
struct lld_sockaddr __attribute__
 This is the SecureBoot Stream type which holds the data for a specific bootloader to HSM call. This packet is needed by HSM the to do the required operation. More...
 

Variable Documentation

◆ h_dest

uint8_t h_dest[ETH_ALEN]

Destination Ethernet address.

◆ h_source

uint8_t h_source[ETH_ALEN]

Source Ethernet address.

◆ h_proto

uint16_t h_proto

Ethernet type in the ethernet frame