AM263Px MCU+ SDK  09.01.00

Detailed Description

Input args for ENET_MDIO_IOCTL_C22_WRITE command.

Clause-22 register write arguments.

Data Fields

EnetMdio_Group group
 
uint32_t phyAddr
 
uint16_t reg
 
uint16_t val
 

Field Documentation

◆ group

EnetMdio_Group EnetMdio_C22WriteInArgs::group

User channel to be used to perform the register access. Simultaneous access from same group is not allowed. Not applicable in manual mode.

◆ phyAddr

uint32_t EnetMdio_C22WriteInArgs::phyAddr

PHY address

◆ reg

uint16_t EnetMdio_C22WriteInArgs::reg

Register address

◆ val

uint16_t EnetMdio_C22WriteInArgs::val

Value to be written