AM263Px MCU+ SDK  09.01.00

Detailed Description

This is a EfuseRowProt type which holds the information of eFuse row index and protection status corresponding to the row index.

Data Fields

uint8_t rowidx
 
uint8_t readProt
 
uint8_t writeProt
 
uint8_t rsvd [1]
 

Field Documentation

◆ rowidx

uint8_t EfuseRowProt_t::rowidx

◆ readProt

uint8_t EfuseRowProt_t::readProt

Index of eFuse row.

◆ writeProt

uint8_t EfuseRowProt_t::writeProt

Read row protection information used in getting or setting an eFuse row protection

◆ rsvd

uint8_t EfuseRowProt_t::rsvd[1]

Write row protection information used in getting or setting an eFuse row protection