AM263Px MCU+ SDK  09.01.00

Detailed Description

ETHPHY device attributes. These are filled by SysCfg based on the PHY device that is selected.

Data Fields

uint32_t mdioBaseAddress
 
uint32_t phyAddress
 

Field Documentation

◆ mdioBaseAddress

uint32_t ETHPHY_Attrs::mdioBaseAddress

Base Address of the MDIO module connected to ETHPHY

◆ phyAddress

uint32_t ETHPHY_Attrs::phyAddress

ETHPHY Address corresponding to MDIO module