AM263Px MCU+ SDK  09.01.00
sdl_mcrc_soc.h File Reference

Go to the source code of this file.

Enumerations

enum  SDL_MCRC_InstType { MCRC0 = 1, SDL_MCRC_INVALID = 0xffff }
 MCRC Instance supported. More...
 

Functions

int32_t SDL_MCRC_getBaseaddr (SDL_MCRC_InstType instance, uint32_t *baseAddr)
 This API is used to get the base address of the instance. More...