AM263Px MCU+ SDK  09.01.00
enet_ioctl.h File Reference

Introduction

This file contains the type definitions and helper macros for the Enet IOCTL interface.

Go to the source code of this file.

Data Structures

struct  Enet_IoctlPrms
 Enet IOCTL param. More...
 
struct  Enet_IoctlValidate
 Enet IOCTL expected param sizes. More...
 

Macros

#define ENET_IOCTL_TYPE_OFFSET   (24U)
 IOCTL type bit offset. More...
 
#define ENET_IOCTL_PER_OFFSET   (16U)
 IOCTL hardware peripheral bit offset. More...
 
#define ENET_IOCTL_MAJOR_OFFSET   (8U)
 IOCTL major number bit offset. More...
 
#define ENET_IOCTL_MINOR_OFFSET   (0U)
 IOCTL minor number bit offset. More...
 
#define ENET_IOCTL_GET_TYPE(x)   ((x) & 0xFF000000U)
 Helper macro to get the IOCTL type (public/private). More...
 
#define ENET_IOCTL_GET_PER(x)   ((x) & 0x00FF0000U)
 Helper macro to get the peripheral type. More...
 
#define ENET_IOCTL_GET_MAJ(x)   ((x) & 0x0000FF00U)
 Helper macro to get the IOCTL major number. More...
 
#define ENET_IOCTL_GET_MIN(x)   ((x) & 0x000000FFU)
 Helper macro to get the IOCTL major number. More...
 
#define ENET_IOCTL_TYPE(x)   ((x) << ENET_IOCTL_TYPE_OFFSET)
 Helper macro to set the IOCTL type. More...
 
#define ENET_IOCTL_PER(x)   ((x) << ENET_IOCTL_PER_OFFSET)
 Helper macro to set the IOCTL type. More...
 
#define ENET_IOCTL_MAJ(x)   ((x) << ENET_IOCTL_MAJOR_OFFSET)
 Helper macro to set the IOCTL major number. More...
 
#define ENET_IOCTL_MIN(x)   ((x) << ENET_IOCTL_MINOR_OFFSET)
 Helper macro to set the IOCTL minor number. More...
 
#define ENET_IOCTL_SET_NO_ARGS(prms)
 Set null args for an IOCTL command that takes no arguments. More...
 
#define ENET_IOCTL_SET_IN_ARGS(prms, in)
 Set the input args for an IOCTL command. More...
 
#define ENET_IOCTL_SET_OUT_ARGS(prms, out)
 Set the output args for an IOCTL command. More...
 
#define ENET_IOCTL_SET_INOUT_ARGS(prms, in, out)
 Set the input and output args for an IOCTL command. More...
 
#define ENET_IOCTL_VALID_PRMS(cmdId, inSize, outSize)
 Helper macro used to add an entry in a IOCTL valid information of type Enet_IoctlValidate. More...
 
#define ENET_IOCTL(hEnet, coreId, ioctlCmd, prms, status)
 Helper macro used to first register IOCTL handler and then invoke the IOCTL. More...
 

Enumerations

enum  Enet_IoctlType_e { ENET_IOCTL_TYPE_PUBLIC = ENET_IOCTL_TYPE(1U), ENET_IOCTL_TYPE_PRIVATE = ENET_IOCTL_TYPE(2U) }
 IOCTL types. More...
 
enum  Enet_IoctlPer_e { ENET_IOCTL_PER_GENERIC = ENET_IOCTL_PER(0U), ENET_IOCTL_PER_CPSW = ENET_IOCTL_PER(1U), ENET_IOCTL_PER_ICSSG = ENET_IOCTL_PER(2U), ENET_IOCTL_PER_GMAC = ENET_IOCTL_PER(3U) }
 IOCTL peripheral types. More...
 
enum  Enet_IoctlMajor_e {
  ENET_IOCTL_PER_BASE = ENET_IOCTL_MAJ(1U), ENET_IOCTL_FDB_BASE = ENET_IOCTL_MAJ(2U), ENET_IOCTL_TIMESYNC_BASE = ENET_IOCTL_MAJ(3U), ENET_IOCTL_HOSTPORT_BASE = ENET_IOCTL_MAJ(4U),
  ENET_IOCTL_MACPORT_BASE = ENET_IOCTL_MAJ(5U), ENET_IOCTL_MDIO_BASE = ENET_IOCTL_MAJ(6U), ENET_IOCTL_STATS_BASE = ENET_IOCTL_MAJ(7U), ENET_IOCTL_PHY_BASE = ENET_IOCTL_MAJ(9U),
  ENET_IOCTL_RM_BASE = ENET_IOCTL_MAJ(10U), ENET_IOCTL_TAS_BASE = ENET_IOCTL_MAJ(11U)
}
 IOCTL base number. More...
 

Functions

static uint32_t Enet_checkInArgs (const Enet_IoctlPrms *prms, uint32_t inArgsSize)
 Check IOCTL input args for commands that expect an input. More...
 
static uint32_t Enet_checkNoInArgs (const Enet_IoctlPrms *prms)
 Check IOCTL input args for commands that don't expect an input. More...
 
static uint32_t Enet_checkOutArgs (const Enet_IoctlPrms *prms, uint32_t outArgsSize)
 Check IOCTL output args for commands that expect an output. More...
 
static uint32_t Enet_checkNoOutArgs (const Enet_IoctlPrms *prms)
 Check IOCTL output args for commands that don't have output. More...
 
static uint32_t Enet_checkInOutArgs (const Enet_IoctlPrms *prms, uint32_t inArgsSize, uint32_t outArgsSize)
 Check IOCTL input and output args. More...