AM263Px MCU+ SDK  09.01.00

Introduction

This file contains the prototype of DTHE driver APIs.

Go to the source code of this file.

Data Structures

struct  DTHE_Attrs
 DTHE attributes. More...
 
struct  DTHE_Config
 DTHE driver context. More...
 

Typedefs

typedef void * DTHE_Handle
 Handle to the DTHE driver. More...
 

Enumerations

enum  DTHE_Return_t { DTHE_RETURN_SUCCESS = 0xCE50311AU, DTHE_RETURN_FAILURE = 0x924FC5E7U }
 DTHE Driver Error code. More...
 

Functions

void DTHE_init (void)
 This function initializes the DTHE. More...
 
void DTHE_deinit (void)
 This function de-initializes the DTHE. More...
 
DTHE_Handle DTHE_open (uint32_t index)
 Function to open DTHE instance, enable DTHE engine. More...
 
DTHE_Return_t DTHE_close (DTHE_Handle handle)
 Function to close a DTHE module specified by the DTHE handle. More...
 

Variables

DTHE_Config gDtheConfig []
 Externally defined driver configuration array. More...
 
uint32_t gDtheConfigNum
 Externally defined driver configuration Num. More...