Data structure used with UART_read() and UART_write()
Data Fields | |
| void * | buf |
| uint32_t | count |
| uint32_t | timeout |
| int32_t | status |
| uint32_t * | args |
| void* UART_Transaction::buf |
[IN] void * to a buffer with data to be transferred . This parameter can't be NULL
| uint32_t UART_Transaction::count |
[IN/OUT] Number of bytes for this transaction. This is input incase of read/write call and on API return this represents number of bytes actually read by the API
| uint32_t UART_Transaction::timeout |
Timeout for this transaction in units of system ticks
| int32_t UART_Transaction::status |
[OUT] UART_TransferStatus code
| uint32_t* UART_Transaction::args |
[IN] Argument to be passed to the callback function