AM261x MCU+ SDK  26.00.00
LLDEnetCfg_t Struct Reference

Detailed Description

Configuration structure for LLDEnet.

Data Fields

uint32_t enetType
 
uint32_t instId
 
void(* txNotifyCb )(void *cbArg)
 
void(* rxNotifyCb )(void *cbArg)
 
void * txCbArg
 
void * rxCbArg
 
uint8_t dstMacAddr [6]
 
uint32_t vlanId
 
uint32_t ethType
 
uint32_t nTxPkts
 
uint32_t nRxPkts [MAX_NUM_RX_DMA_CH_PER_INSTANCE]
 
uint32_t pktSize
 
int dmaTxChId
 
int dmaRxChId [MAX_NUM_RX_DMA_CH_PER_INSTANCE]
 
bool unusedDmaRx
 
bool unusedDmaTx
 
bool dmaTxShared
 
bool dmaRxShared
 
bool dmaRxOwner
 
uint32_t numRxChannels
 

Field Documentation

◆ enetType

uint32_t LLDEnetCfg_t::enetType

Ethernet type.

◆ instId

uint32_t LLDEnetCfg_t::instId

Instance ID.

◆ txNotifyCb

void(* LLDEnetCfg_t::txNotifyCb) (void *cbArg)

Transmit notification callback function pointer.

◆ rxNotifyCb

void(* LLDEnetCfg_t::rxNotifyCb) (void *cbArg)

Receive notification callback function pointer.

◆ txCbArg

void* LLDEnetCfg_t::txCbArg

Argument to be passed to the transmit notification callback function.

◆ rxCbArg

void* LLDEnetCfg_t::rxCbArg

Argument to be passed to the receive notification callback function.

◆ dstMacAddr

uint8_t LLDEnetCfg_t::dstMacAddr[6]

Destination MAC address to filter RX packets. If all bytes of MAC addres are 0, no filter is applied.

◆ vlanId

uint32_t LLDEnetCfg_t::vlanId

VLAN ID to filter RX packets. If all bytes of dstMacAddr are 0, no filter is applied.

◆ ethType

uint32_t LLDEnetCfg_t::ethType

Ethernet Type to filter RX packets.

◆ nTxPkts

uint32_t LLDEnetCfg_t::nTxPkts

Number of buffers allocated for transmit packets Set to 0 to use the default value assigned by the implementation.

◆ nRxPkts

uint32_t LLDEnetCfg_t::nRxPkts[MAX_NUM_RX_DMA_CH_PER_INSTANCE]

Number of buffers allocated for receive packets Set to 0 to use the default value assigned by the implementation.

◆ pktSize

uint32_t LLDEnetCfg_t::pktSize

Transmit and receive maximum packet size. Set to 0 to use the default value assigned by the implementation.

◆ dmaTxChId

int LLDEnetCfg_t::dmaTxChId

DMA transmit channel ID. Set to -1 for dynamic allocation, only supported by Jacinto.

◆ dmaRxChId

int LLDEnetCfg_t::dmaRxChId[MAX_NUM_RX_DMA_CH_PER_INSTANCE]

DMA receive channel ID. Set to -1 for dynamic allocation, only supported by Jacinto.

◆ unusedDmaRx

bool LLDEnetCfg_t::unusedDmaRx

true: won't use DMA RX; false: will use DMA RX This is used when there is no interest in receiving data.

◆ unusedDmaTx

bool LLDEnetCfg_t::unusedDmaTx

true: won't use DMA TX; false: will use DMA TX This is used when there is no interest in sending data.

◆ dmaTxShared

bool LLDEnetCfg_t::dmaTxShared

Only the Sitara supports this param. true: the dmaTxChId is shared between apps; false: not shared

◆ dmaRxShared

bool LLDEnetCfg_t::dmaRxShared

Only the Sitara AM273x supports this param. true: the dmaRxChId is shared between apps; false: not shared

◆ dmaRxOwner

bool LLDEnetCfg_t::dmaRxOwner

Only the Sitara AM273x supports this param. true: the LLDEnet_t owns this RX DMA channel, it has the full permission to access the SDK DMA API; false: the LLDEnet_t is unable to to call SDK RX DMA API This is used when there are multiple LLDEnet_t shares the same DMA RX channel. User has to make sure only one LLDEnet_t has dmaRxOwner is set to true if the DMA channel share function is used.

◆ numRxChannels

uint32_t LLDEnetCfg_t::numRxChannels

Number of Rx DMA channels, only ICSSG peripheral has more than 1 Rx DMA channels.