AM261x MCU+ SDK  26.00.00
I2CLLD_Transaction Struct Reference

Detailed Description

I2C Transaction.

This structure defines the nature of the I2C transaction.

I2C Controller Mode: This structure specifies the buffer and buffer's size that is to be written to and read from the I2C target peripheral.

Data Fields

uint8_t * writeBuf
 
uint32_t writeCount
 
uint8_t * readBuf
 
uint32_t readCount
 

Field Documentation

◆ writeBuf

uint8_t* I2CLLD_Transaction::writeBuf

[IN] Data buffer from which data to be written to the target

◆ writeCount

uint32_t I2CLLD_Transaction::writeCount

[IN] Number of bytes to be written to the target

◆ readBuf

uint8_t* I2CLLD_Transaction::readBuf

[IN] Data buffer to which data to be read from the target

◆ readCount

uint32_t I2CLLD_Transaction::readCount

[IN] Number of bytes to be read from the target