AM261x MCU+ SDK  26.00.00
sdl_soc_ccm.h File Reference

Go to the source code of this file.

Macros

#define SDL_CCM_ESM_U_BASE   (SDL_ESM0_CCM_0_SELFTEST_ERR)
 
#define SDL_INTR_GROUP_NUM   1U
 
#define BASEADDRESS   SDL_R5SS0_CCMR_U_BASE
 
#define ESM_INSTANCE   SDL_ESM_INST_MAIN_ESM0
 
#define SDL_R5SS0_CCM   0U
 
#define SDL_CCM_MAX_INSTANCE   (SDL_R5SS0_CCM + 1U)
 

Typedefs

typedef uint32_t SDL_CCM_Inst
 CCM Instance supported. More...
 

Variables

static uint32_t SDL_CCM_baseAddress [SDL_CCM_MAX_INSTANCE]
 This API is used to get the base address of the instance. More...