AM261x MCU+ SDK  26.00.00
Timer and events utility functions

Introduction

Files

file  cb_tmevent.h
 Timer and events utility functions.
 

Functions

static int cb_nanosleep64 (int64_t ts64, int64_t *rts64)
 nano second unit sleep More...
 
cb_timer_object_t * cb_timer_create (char *tname)
 creates timer. More...
 
void cb_timer_close (cb_timer_object_t *mtmo)
 close the timer More...
 
int cb_timer_start_interval (cb_timer_object_t *mtmo, uint32_t value_ms, uint32_t interval_ms)
 start timer interval. More...
 
int cb_timer_stop (cb_timer_object_t *mtmo)
 timer stop. More...
 
bool cb_timer_expired (cb_timer_object_t *mtmo, cb_timer_clear_t clear)
 timer expired More...
 

Typedefs

typedef struct cb_timer_object cb_timer_object_t
 handler for cb_timer_object More...
 

Enumerations

enum  cb_timer_clear_t { CB_TIMER_NO_CLEAR, CB_TIMER_DECREMENT, CB_TIMER_ALL_CLEAR }
 enumeration used for timer to clear, decrement or no clear. This enumeration has following members: More...
 

Macros

#define CB_USLEEP(x)   usleep(x)
 micro second unit sleep More...
 
#define CB_SLEEP(x)   sleep(x)
 second unit sleep More...
 
#define CB_MKTIME(x)   mktime(x)
 seconds since the Epoch, 1970-01-01 00:00:00 +0000 (UTC) More...
 

Macro Definition Documentation

◆ CB_USLEEP

#define CB_USLEEP (   x)    usleep(x)

micro second unit sleep

◆ CB_SLEEP

#define CB_SLEEP (   x)    sleep(x)

second unit sleep

◆ CB_MKTIME

#define CB_MKTIME (   x)    mktime(x)

seconds since the Epoch, 1970-01-01 00:00:00 +0000 (UTC)

Typedef Documentation

◆ cb_timer_object_t

typedef struct cb_timer_object cb_timer_object_t

handler for cb_timer_object

Note
cb_timer is signal event based timer, no thread, no callback happens with this. users need to call 'cb_timer_expired' to check the configured timer

Enumeration Type Documentation

◆ cb_timer_clear_t

enumeration used for timer to clear, decrement or no clear. This enumeration has following members:

  1. CB_TIMER_NO_CLEAR -> no action on timer value
  2. CB_TIMER_DECREMENT -> timer value decrement
  3. CB_TIMER_ALL_CLEAR -> set timer value to 0.
Enumerator
CB_TIMER_NO_CLEAR 
CB_TIMER_DECREMENT 
CB_TIMER_ALL_CLEAR 

Function Documentation

◆ cb_nanosleep64()

static int cb_nanosleep64 ( int64_t  ts64,
int64_t *  rts64 
)
inlinestatic

nano second unit sleep

◆ cb_timer_create()

cb_timer_object_t* cb_timer_create ( char *  tname)

creates timer.

Parameters
tnametimer name
Returns
hanler of cb_timer_object_t

◆ cb_timer_close()

void cb_timer_close ( cb_timer_object_t *  mtmo)

close the timer

Parameters
mtmoreference to cb_timer_object_t, returned by cb_timer_create().

◆ cb_timer_start_interval()

int cb_timer_start_interval ( cb_timer_object_t *  mtmo,
uint32_t  value_ms,
uint32_t  interval_ms 
)

start timer interval.

Parameters
mtmoreference to cb_timer_object_t, created and returned by cb_timer_create().
value_msinitial value in msec.
interval_mstime interval in msec.
Returns
0 on success, -1 on error
Note
both value_ms and interval_ms is used by timer_settime.

◆ cb_timer_stop()

int cb_timer_stop ( cb_timer_object_t *  mtmo)

timer stop.

Parameters
mtmoreference to cb_timer_object_t, which is created and returned by cb_timer_create().
Returns
0 on success, -1 on error.

◆ cb_timer_expired()

bool cb_timer_expired ( cb_timer_object_t *  mtmo,
cb_timer_clear_t  clear 
)

timer expired

Parameters
mtmoreference to cb_timer_object_t, which is created and returned by cb_timer_create().
clearaction by the definition of cb_timer_clear_t
Returns
true if timer not expired, false if timer expired.