AM261x MCU+ SDK  26.00.00

Introduction

This module contains APIs for optimized trignometric functions.

Functions

float ti_arm_sin (float angleRad)
 Computes the trigonometric sine value of the input angle using polynomial approximation techniques. More...
 
float ti_arm_cos (float angleRad)
 Computes the trigonometric cosine value of the input angle using polynomial approximation techniques. More...
 
void ti_arm_sincos (float angleRad, float *retValues)
 Computes the trigonometric sine and cosine values of the input angle using polynomial approximation techniques. More...
 
float ti_arm_asin (float x)
 Computes the trigonometric arcsine value of the input value using polynomial approximation techniques. More...
 
float ti_arm_acos (float x)
 Computes the trigonometric arccosine value of the input value using polynomial approximation techniques. More...
 
float ti_arm_atan (float x)
 Computes the trigonometric arctangent value of the input value using polynomial approximation techniques. More...
 
float ti_arm_atan2 (float y, float x)
 Computes the trigonometric atan2 value of the input values using polynomial approximation techniques. More...
 
static TRIG_TEXT_SECTION float ti_arm_sqrt (float x)
 Arm FPU Hardware Single-Precision Square Root Function. More...
 
static TRIG_TEXT_SECTION float ti_arm_abs (float x)
 Arm FPU Hardware Single-Precision Absolute Value Function. More...
 

Macros

#define TRIG_TEXT_SECTION   __attribute__((section(".trigText"))) __attribute__((always_inline))
 
#define TRIG_DATA_SECTION   __attribute__((aligned(8), section(".trigData")))
 

Macro Definition Documentation

◆ TRIG_TEXT_SECTION

#define TRIG_TEXT_SECTION   __attribute__((section(".trigText"))) __attribute__((always_inline))

◆ TRIG_DATA_SECTION

#define TRIG_DATA_SECTION   __attribute__((aligned(8), section(".trigData")))

Function Documentation

◆ ti_arm_sin()

float ti_arm_sin ( float  angleRad)

Computes the trigonometric sine value of the input angle using polynomial approximation techniques.

Parameters
[in]angleRad- input angle in radians within [0, 2PI]
Returns
Computed sine value
Note
Usage Considerations: Valid input is limited to values between 0 to 2PI. Add 2PI to negative values before calling this function. No error checking is performed on input.

◆ ti_arm_cos()

float ti_arm_cos ( float  angleRad)

Computes the trigonometric cosine value of the input angle using polynomial approximation techniques.

Parameters
[in]angleRad- - input angle in radians within [0, 2PI]
Returns
Computed cosine value
Note
Usage Considerations: Valid input is limited to values between 0 to 2PI. Add 2PI to negative values before calling this function. No error checking is performed on input.

◆ ti_arm_sincos()

void ti_arm_sincos ( float  angleRad,
float *  retValues 
)

Computes the trigonometric sine and cosine values of the input angle using polynomial approximation techniques.

Parameters
[in]angleRad- - input angle in radians
[out]retValues- points to the computed sine and cosine values.
Note
Usage Considerations: Valid input is limited to values between 0 to 2PI. Add 2PI to negative values before calling this function. No error checking is performed on input.

◆ ti_arm_asin()

float ti_arm_asin ( float  x)

Computes the trigonometric arcsine value of the input value using polynomial approximation techniques.

Parameters
[in]x- input value within the domain of arcsine
Returns
Computed arcsine value
Note
Usage Considerations: Valid input is limited to values within the domain of arcsine, [-1, 1]. No error checking is performed on input.

◆ ti_arm_acos()

float ti_arm_acos ( float  x)

Computes the trigonometric arccosine value of the input value using polynomial approximation techniques.

Parameters
[in]x- input value within the domain of arccosine
Returns
Computed arccosine value
Note
Usage Considerations: Valid input is limited to values within the domain of arccosine, [-1, 1]. No error checking is performed on input.

◆ ti_arm_atan()

float ti_arm_atan ( float  x)

Computes the trigonometric arctangent value of the input value using polynomial approximation techniques.

Parameters
[in]x- input value within the domain of arctangent
Returns
Computed arctangent value
Note
Usage Considerations: No error checking is performed on input.

◆ ti_arm_atan2()

float ti_arm_atan2 ( float  y,
float  x 
)

Computes the trigonometric atan2 value of the input values using polynomial approximation techniques.

Parameters
[in]x- input value within the domain of arctangent
[in]y- input value within the domain of arctangent
Returns
Computed atan2 value
Note
Usage Considerations: No error checking is performed on input.

◆ ti_arm_sqrt()

static TRIG_TEXT_SECTION float ti_arm_sqrt ( float  x)
inlinestatic

Arm FPU Hardware Single-Precision Square Root Function.

Parameters
[in]x- input value
Returns
Square root of an input number

◆ ti_arm_abs()

static TRIG_TEXT_SECTION float ti_arm_abs ( float  x)
inlinestatic

Arm FPU Hardware Single-Precision Absolute Value Function.

Parameters
[in]x- input value
Returns
Absolute value of an input number