AM261x MCU+ SDK  26.00.00

Introduction

This module contains APIs to program and use the Ram module on the board like GPMC pSRAM. See RAM for more details.

Data Structures

struct  Ram_DevConfig
 
struct  Ram_Attrs
 
struct  Ram_Fxns
 Driver implementation callbacks. More...
 
struct  Ram_Config
 Ram driver configuration, these are filled by SysCfg based on the ram device that is selected. More...
 
struct  Ram_Params
 Parameters passed during RAM_open() More...
 

Functions

Ram_Attrs * Ram_getAttrs (uint32_t instanceId)
 
Ram_Handle Ram_open (uint32_t instanceId, Ram_Params *params)
 Open RAM driver. More...
 
void Ram_close (Ram_Handle handle)
 Close RAM driver. More...
 
int32_t Ram_write (Ram_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Write to RAM device. More...
 
int32_t Ram_read (Ram_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Read data from RAM device. More...
 

Typedefs

typedef void * Ram_Handle
 Handle to the RAM driver returned by Ram_open() More...
 
typedef struct Ram_Config_s Ram_Config
 Forward declaration of Ram_Config. More...
 
typedef struct Ram_Params_s Ram_Params
 Forward declaration of Ram_Params. More...
 

RAM driver implementation callbacks

typedef int32_t(* Ram_OpenFxn) (Ram_Config *config)
 Driver implementation to open a specific RAM driver. More...
 
typedef void(* Ram_CloseFxn) (Ram_Config *config)
 Driver implementation to close a specific RAM driver. More...
 
typedef int32_t(* Ram_ReadFxn) (Ram_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to read from RAM using a specific RAM driver. More...
 
typedef int32_t(* Ram_WriteFxn) (Ram_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
 Driver implementation to write to RAM using specific RAM driver. More...
 
typedef int32_t(* Ram_quirksFxn) (Ram_Config *config)
 Ram device config. This will be part of the ram config, so has to be filled by sysconfig or otherwise before invoking Ram_open. More...
 
typedef int32_t(* Ram_custProtocolFxn) (Ram_Config *config)
 User implementation of a custom function to configure RAM to operate in a specific protocol. More...
 

Typedef Documentation

◆ Ram_Handle

typedef void* Ram_Handle

Handle to the RAM driver returned by Ram_open()

◆ Ram_Config

typedef struct Ram_Config_s Ram_Config

Forward declaration of Ram_Config.

◆ Ram_Params

typedef struct Ram_Params_s Ram_Params

Forward declaration of Ram_Params.

◆ Ram_OpenFxn

typedef int32_t(* Ram_OpenFxn) (Ram_Config *config)

Driver implementation to open a specific RAM driver.

Typically this callback is hidden from the end application and is implemented when a new type of RAM device needs to be implemented.

Parameters
config[in] RAM configuration for the specific RAM device
Returns
SystemP_SUCCESS on success, else failure

◆ Ram_CloseFxn

typedef void(* Ram_CloseFxn) (Ram_Config *config)

Driver implementation to close a specific RAM driver.

Typically this callback is hidden from the end application and is implemented when a new type of RAM device needs to be implemented.

Parameters
config[in] RAM configuration for the specific RAM device
Returns
SystemP_SUCCESS on success, else failure

◆ Ram_ReadFxn

typedef int32_t(* Ram_ReadFxn) (Ram_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)

Driver implementation to read from RAM using a specific RAM driver.

Typically this callback is hidden from the end application and is implemented when a new type of RAM device needs to be implemented.

Parameters
config[in] RAM configuration for the specific RAM device
offset[in] Offset in the RAM from where to start the read
buf[in] Buffer into which to read the data into
len[in] Length of the data to read, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Ram_WriteFxn

typedef int32_t(* Ram_WriteFxn) (Ram_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)

Driver implementation to write to RAM using specific RAM driver.

Typically this callback is hidden from the end application and is implemented when a new type of RAM device needs to be implemented.

Parameters
config[in] RAM configuration for the specific RAM device
offset[in] Offset in the RAM from where to start the write.
buf[in] Buffer which has the data to write.
len[in] Length of the data to write, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Ram_quirksFxn

typedef int32_t(* Ram_quirksFxn) (Ram_Config *config)

Ram device config. This will be part of the ram config, so has to be filled by sysconfig or otherwise before invoking Ram_open.

User implementation of a custom function to handle vendor specific quirks

Typically this callback is hidden from the end application and is implemented when a new type of RAM device needs to be implemented.

Parameters
config[in] RAM configuration for the specific RAM device
Returns
SystemP_SUCCESS on success, else failure

◆ Ram_custProtocolFxn

typedef int32_t(* Ram_custProtocolFxn) (Ram_Config *config)

User implementation of a custom function to configure RAM to operate in a specific protocol.

Parameters
config[in] RAM configuration for the specific RAM device
Returns
SystemP_SUCCESS on success, else failure

Function Documentation

◆ Ram_getAttrs()

Ram_Attrs* Ram_getAttrs ( uint32_t  instanceId)

◆ Ram_open()

Ram_Handle Ram_open ( uint32_t  instanceId,
Ram_Params *  params 
)

Open RAM driver.

Make sure the SOC peripheral driver is opened before calling this API. Drivers_open function generated by SysCfg opens the underlying SOC peripheral driver, e.g OSPI.

Global variables RAM_Config gRAMConfig[] and uint32_t gRAMConfigNum is instantiated by SysCfg to describe the RAM configuration based on user selection in SysCfg.

Parameters
instanceId[in] Index within RAM_Config gRAMConfig[] denoting the RAM driver to open
params[in] Open parameters
Returns
Handle to RAM driver which should be used in subsequent API call
NULL in case of failure

◆ Ram_close()

void Ram_close ( Ram_Handle  handle)

Close RAM driver.

Parameters
handle[in] RAM driver handle from Ram_open

◆ Ram_write()

int32_t Ram_write ( Ram_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

Write to RAM device.

Parameters
handle[in] RAM driver handle from Ram_open
offset[in] Offset in the RAM from where to start the write.
buf[in] Buffer which has the data to write.
len[in] Length of the data to write, in bytes
Returns
SystemP_SUCCESS on success, else failure

◆ Ram_read()

int32_t Ram_read ( Ram_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

Read data from RAM device.

Parameters
handle[in] RAM driver handle from Ram_open
offset[in] Offset in the RAM from where to start the read
buf[in] Buffer into which to read the data into
len[in] Length of the data to read, in bytes
Returns
SystemP_SUCCESS on success, else failure