|
| static void | dwc_usb3_do_setup (dwc_usb3_pcd_t *pcd) |
| | This routine processes SETUP commands. The USB Command processing is done in two places - the first being the PCD and the second being the Gadget driver (for example, the File-Backed Storage Gadget driver). More...
|
| |
| static void | ep0_do_stall (dwc_usb3_pcd_t *pcd, int err_val) |
| | This routine stalls EP0. More...
|
| |
| static void | do_clear_halt (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep) |
| | Clear the EP halt (STALL), and if there are pending requests start the transfer. More...
|
| |
| static void | do_get_status (dwc_usb3_pcd_t *pcd) |
| | This routine processes the GET_STATUS Setup Commands. More...
|
| |
| static void | do_clear_feature (dwc_usb3_pcd_t *pcd) |
| | This routine processes the CLEAR_FEATURE Setup Commands. More...
|
| |
| static void | do_set_feature (dwc_usb3_pcd_t *pcd) |
| | This routine processes the SET_FEATURE Setup Commands. More...
|
| |
| static void | do_set_address (dwc_usb3_pcd_t *pcd) |
| | This routine processes the SET_ADDRESS Setup Commands. More...
|
| |
| static void | do_get_descriptor (dwc_usb3_pcd_t *pcd) |
| | This routine handles the Get Descriptor request for the BOS descriptor and the OTG descriptor, and passes all other requests to the Gadget driver. More...
|
| |
| static void | ep0_continue_transfer (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_req_t *req) |
| | This routine continues control IN transfers started by ep0_start_transfer, when the transfer does not fit in a single request. More...
|
| |
| static int | ep0_complete_request (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_req_t *req, dwc_usb3_dma_desc_t *desc, int status) |
| | This routine completes the ep0 control transfer. More...
|
| |
| static void | setup_in_status_phase (dwc_usb3_pcd_t *pcd, void *buf, dwc_dma_t dma) |
| | This routine starts the Zero-Length Packet for the IN status phase of a control write transfer. More...
|
| |
| static void | setup_out_status_phase (dwc_usb3_pcd_t *pcd, void *buf, dwc_dma_t dma) |
| | This routine starts the Zero-Length Packet for the OUT status phase of a control read transfer. More...
|
| |
| static void | dwc_usb3_handle_ep0 (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_req_t *req, u32 event) |
| | This routine handles EP0 Control transfers. More...
|
| |
| void | dwc_usb3_pcd_ep0_data_stage (dwc_usb3_pcd_t *pcd, int length) |
| | This routine starts the data stage of a 3-stage control command. pcd->ep0state must be set to EP0_OUT_DATA_PHASE or EP0_IN_DATA_PHASE, and pcd->ep0->dwc_ep.is_in must be set to 0 or 1 before calling this routine. For IN, the data to be sent must be placed in pcd->ep0_status_buf before the call. More...
|
| |
| void | dwc_usb3_handle_ep0_xfer (dwc_usb3_pcd_t *pcd, u32 event) |
| | This routine handles EP0 transfers. More...
|
| |