AM261x MCU+ SDK  26.00.00
dwc_queue.h File Reference

Introduction

DWC queue implementation.

Go to the source code of this file.

Data Structures

struct  dwc_queue_t
 A structure representing a queue for managing data. More...
 

Macros

#define DWC_QUEUE_SIZE   (8U)
 

Functions

void dwc_queueInit (dwc_queue_t *queue)
 This routine initializes the queue. More...
 
bool dwc_queuePut (dwc_queue_t *queue, uint32_t data)
 This routine adds an element to the queue. More...
 
bool dwc_queueGet (dwc_queue_t *queue, uint32_t *data)
 This routine retrieves an elements from the queue. More...
 

Macro Definition Documentation

◆ DWC_QUEUE_SIZE

#define DWC_QUEUE_SIZE   (8U)

============================================================================