AM261x MCU+ SDK  26.00.00
bootloader_soc.h File Reference

Go to the source code of this file.

Data Structures

struct  Bootloader_CoreBootInfo
 Data structure containing information about a core specific to the SOC. More...
 
struct  Bootloader_socCoreOpModeConfig
 Data structure containing information about the operating mode specific to the SOC. More...
 

Macros

#define BOOTLOADER_APP_SEGMENT_CANBE_ENCRYPTED   (0xA5U)
 
#define BOOTLOADER_APP_SEGMENT_CANNOTBE_ENCRYPTED   (0x5AU)
 
#define BOOTLOADER_SOC_APP_CERT_SIZE   (0x1000)
 
Device Types

#define BOOTLOADER_DEVTYPE_HSSE   (0x0AU)
 device type HSSE More...
 
#define BOOTLOADER_DEVTYPE_HSFS   (0xAAU)
 device type HSFS More...
 
#define BOOTLOADER_DEVTYPE_GP   (0x03U)
 device type GP
More...
 
#define BOOTLOADER_CLIENT_ID   (0x02)
 hsmclient ID for bootloader More...
 
#define BOOTLOADER_MAX_SBL_SIZE_IN_TCM_KB   (640U)
 

Functions

int32_t Bootloader_socCpuRequest (uint32_t cpuId)
 Request for a particular CPU in the AM64x SOC. More...
 
int32_t Bootloader_socCpuRelease (uint32_t cpuId)
 Release a particular CPU in the AM64x SOC. More...
 
int32_t Bootloader_socCpuSetClock (uint32_t cpuId, uint32_t cpuHz)
 Set the clock of a particular CPU in the AM64x SOC. More...
 
uint64_t Bootloader_socCpuGetClock (uint32_t cpuId)
 Get the clock of a particular CPU in the AM64x SOC. More...
 
uint32_t Bootloader_socCpuGetClkDefault (uint32_t cpuId)
 Get the default clock of a particular CPU in the AM64x SOC. More...
 
int32_t Bootloader_socCpuPowerOnReset (uint32_t cpuId, void *socCoreOpMode)
 Do power-on-reset of a particular CPU in the AM64x SOC. More...
 
int32_t Bootloader_socCpuResetRelease (uint32_t cpuId, uintptr_t entryPoint)
 Release a particular CPU in the AM64x SOC from reset. More...
 
int32_t Bootloader_socCpuResetReleaseSelf (void)
 Release self CPU in the AM64x SOC from reset. More...
 
int32_t Bootloader_socCpuSetEntryPoint (uint32_t cpuId, uintptr_t entryPoint)
 Set entry point for self CPU in the AM64x SOC from reset. More...
 
uint32_t Bootloader_socTranslateSectionAddr (uint32_t cslCoreId, uint32_t addr)
 Translate a CPU address to the SOC address wherever applicable. More...
 
uint32_t Bootloader_socRprcToCslCoreId (uint32_t rprcCoreId)
 Obtain the CSL core ID of a CPU from its RPRC core ID. More...
 
uint32_t * Bootloader_socGetSelfCpuList (void)
 Get the list of self cpus in the SOC. More...
 
char * Bootloader_socGetCoreName (uint32_t cpuId)
 Get the name of a core. More...
 
int32_t Bootloader_socMemInitCpu (uint32_t cpuId)
 Initialize the core memories of a specific core. More...
 
int32_t Bootloader_socSecHandover (void)
 API to trigger the security handover from SYSFW. More...
 
void Bootloader_socInitL2MailBoxMemory (void)
 API to configure Core and Per PLLS. More...
 
int32_t Bootloader_socAuthImage (uint32_t certLoadAddr)
 API to authenticate (and decrypt if needed) an appimage using SYSFW. More...
 
uint32_t Bootloader_socIsAuthRequired (void)
 API to check if authentication is required for the device. Checks the SYS_STATUS register to see if device is GP, HS-FS, HS-SE etc. More...
 
void Bootloader_socGetBootSeqOid (uint8_t *boot_seq_oid)
 API to get boot sequence oid. More...
 
void Bootloader_socLoadHsmRtFw (HsmClient_t *gHSMClient, const uint8_t *HsmRtFw, uint32_t hsmRTSize)
 API to load hsm runtime firmware. More...
 
void Bootloader_socLoadHsmRtFwNonBlocking (HsmClient_t *gHSMClient, const uint8_t *HsmRtFw, uint32_t hsmRTSize)
 Non blocking API to load hsm runtime firmware. More...
 
void Bootloader_socSetAutoClock ()
 API to set CPU clock to 200 MHz or 400 MHz on the basis of eFUSE bits configuration. More...
 
int32_t Bootloader_socCpuSetAppEntryPoint (uint32_t cpuId, uintptr_t entryPoint)
 
int32_t Bootloader_authStart (uintptr_t startAddr, uint32_t size)
 API to start streaming boot authentication. More...
 
int32_t Bootloader_authUpdate (uintptr_t startAddr, uint32_t size, uint8_t enc)
 API to update the Secure Boot Stream with a new segment. More...
 
int32_t Bootloader_authFinish (void)
 API to finish streaming boot authentication. More...
 

Macro Definition Documentation

◆ BOOTLOADER_APP_SEGMENT_CANBE_ENCRYPTED

#define BOOTLOADER_APP_SEGMENT_CANBE_ENCRYPTED   (0xA5U)

This application segment can be encrypted.

◆ BOOTLOADER_APP_SEGMENT_CANNOTBE_ENCRYPTED

#define BOOTLOADER_APP_SEGMENT_CANNOTBE_ENCRYPTED   (0x5AU)

This application segment can never be encrypted.

◆ BOOTLOADER_SOC_APP_CERT_SIZE

#define BOOTLOADER_SOC_APP_CERT_SIZE   (0x1000)

Maximum supported size of the application certificate

◆ BOOTLOADER_DEVTYPE_HSSE

#define BOOTLOADER_DEVTYPE_HSSE   (0x0AU)

device type HSSE

◆ BOOTLOADER_DEVTYPE_HSFS

#define BOOTLOADER_DEVTYPE_HSFS   (0xAAU)

device type HSFS

◆ BOOTLOADER_DEVTYPE_GP

#define BOOTLOADER_DEVTYPE_GP   (0x03U)

device type GP

◆ BOOTLOADER_CLIENT_ID

#define BOOTLOADER_CLIENT_ID   (0x02)

hsmclient ID for bootloader

◆ BOOTLOADER_MAX_SBL_SIZE_IN_TCM_KB

#define BOOTLOADER_MAX_SBL_SIZE_IN_TCM_KB   (640U)

The maximum size of the SBL in TCM memory : Derived from ROM Eclipse

Function Documentation

◆ Bootloader_socCpuRequest()

int32_t Bootloader_socCpuRequest ( uint32_t  cpuId)

Request for a particular CPU in the AM64x SOC.

This API internally makes Sciclient calls to request control of the CPU

Parameters
cpuId[in] The CSL ID of the core
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socCpuRelease()

int32_t Bootloader_socCpuRelease ( uint32_t  cpuId)

Release a particular CPU in the AM64x SOC.

This API internally makes Sciclient calls to release control of the CPU

Parameters
cpuId[in] The CSL ID of the core
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socCpuSetClock()

int32_t Bootloader_socCpuSetClock ( uint32_t  cpuId,
uint32_t  cpuHz 
)

Set the clock of a particular CPU in the AM64x SOC.

This API internally makes Sciclient calls to set CPU clock

Parameters
cpuId[in] The CSL ID of the core
cpuHz[in] Desired clock frequency of the CPU in Hertz
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socCpuGetClock()

uint64_t Bootloader_socCpuGetClock ( uint32_t  cpuId)

Get the clock of a particular CPU in the AM64x SOC.

This API internally makes Sciclient calls to get the current clock frequency of CPU

Parameters
cpuId[in] The CSL ID of the core
Returns
Current clock speed of the CPU

◆ Bootloader_socCpuGetClkDefault()

uint32_t Bootloader_socCpuGetClkDefault ( uint32_t  cpuId)

Get the default clock of a particular CPU in the AM64x SOC.

This API queries and internal lookup table to fetch the default clock speed at which a particular CPU should run.

Parameters
cpuId[in] The CSL ID of the core
Returns
Default clock speed of the CPU

◆ Bootloader_socCpuPowerOnReset()

int32_t Bootloader_socCpuPowerOnReset ( uint32_t  cpuId,
void *  socCoreOpMode 
)

Do power-on-reset of a particular CPU in the AM64x SOC.

This API is called only when booting a non-self CPU.

Parameters
cpuId[in] The CSL ID of the core
Returns
SystemP_SUCCESS on success, else failure
Parameters
socCoreOpModeLockstep/Dual core mode as per setting in syscfg.

◆ Bootloader_socCpuResetRelease()

int32_t Bootloader_socCpuResetRelease ( uint32_t  cpuId,
uintptr_t  entryPoint 
)

Release a particular CPU in the AM64x SOC from reset.

This API is called only when booting a non-self CPU. There is a different API Bootloader_socCpuResetReleaseSelf in the case of a self CPU

Parameters
cpuId[in] The CSL ID of the core
entryPoint[in] The entryPoint of the CPU, from where it should start execution
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socCpuResetReleaseSelf()

int32_t Bootloader_socCpuResetReleaseSelf ( void  )

Release self CPU in the AM64x SOC from reset.

Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socCpuSetEntryPoint()

int32_t Bootloader_socCpuSetEntryPoint ( uint32_t  cpuId,
uintptr_t  entryPoint 
)

Set entry point for self CPU in the AM64x SOC from reset.

This API need not be called when booting a non-self CPU. The entry point can be specified in the Bootloader_socCpuResetRelease function itself

Parameters
cpuId[in] The CSL ID of the core
entryPoint[in] The entryPoint of the CPU, from where it should start execution
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socTranslateSectionAddr()

uint32_t Bootloader_socTranslateSectionAddr ( uint32_t  cslCoreId,
uint32_t  addr 
)

Translate a CPU address to the SOC address wherever applicable.

This API need not be called when booting a non-self CPU. The entry point can be specified in the Bootloader_socCpuResetRelease function itself

Parameters
cslCoreId[in] The CSL ID of the core
addr[in] The CPU addr
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socRprcToCslCoreId()

uint32_t Bootloader_socRprcToCslCoreId ( uint32_t  rprcCoreId)

Obtain the CSL core ID of a CPU from its RPRC core ID.

Parameters
rprcCoreId[in] The RPRC ID of the core
Returns
CSL core ID of a CPU

◆ Bootloader_socGetSelfCpuList()

uint32_t* Bootloader_socGetSelfCpuList ( void  )

Get the list of self cpus in the SOC.

Returns
List of self cpus ending with an invalid core id

◆ Bootloader_socGetCoreName()

char* Bootloader_socGetCoreName ( uint32_t  cpuId)

Get the name of a core.

Parameters
cpuId[in] The CSL ID of the core
Returns
Name of the CPU

◆ Bootloader_socMemInitCpu()

int32_t Bootloader_socMemInitCpu ( uint32_t  cpuId)

Initialize the core memories of a specific core.

Parameters
cpuId[in] The CSL ID of the core
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socSecHandover()

int32_t Bootloader_socSecHandover ( void  )

API to trigger the security handover from SYSFW.

Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socInitL2MailBoxMemory()

void Bootloader_socInitL2MailBoxMemory ( void  )

API to configure Core and Per PLLS.

API to Init L2,L3 Banks and Mailbox Memory

◆ Bootloader_socAuthImage()

int32_t Bootloader_socAuthImage ( uint32_t  certLoadAddr)

API to authenticate (and decrypt if needed) an appimage using SYSFW.

Parameters
certLoadAddr[in] The SOC address pointing to the certificate+appimage
Returns
SystemP_SUCCESS on success, else failure

◆ Bootloader_socIsAuthRequired()

uint32_t Bootloader_socIsAuthRequired ( void  )

API to check if authentication is required for the device. Checks the SYS_STATUS register to see if device is GP, HS-FS, HS-SE etc.

Returns
TRUE (1U) if authentication required, FALSE (0U) if not.

◆ Bootloader_socGetBootSeqOid()

void Bootloader_socGetBootSeqOid ( uint8_t *  boot_seq_oid)

API to get boot sequence oid.

Parameters
boot_seq_oid[in] pointer to integer array for populating boot sequence oid

◆ Bootloader_socLoadHsmRtFw()

void Bootloader_socLoadHsmRtFw ( HsmClient_t *  gHSMClient,
const uint8_t *  HsmRtFw,
uint32_t  hsmRTSize 
)

API to load hsm runtime firmware.

◆ Bootloader_socLoadHsmRtFwNonBlocking()

void Bootloader_socLoadHsmRtFwNonBlocking ( HsmClient_t *  gHSMClient,
const uint8_t *  HsmRtFw,
uint32_t  hsmRTSize 
)

Non blocking API to load hsm runtime firmware.

◆ Bootloader_socSetAutoClock()

void Bootloader_socSetAutoClock ( )

API to set CPU clock to 200 MHz or 400 MHz on the basis of eFUSE bits configuration.

◆ Bootloader_socCpuSetAppEntryPoint()

int32_t Bootloader_socCpuSetAppEntryPoint ( uint32_t  cpuId,
uintptr_t  entryPoint 
)

dummy api call

◆ Bootloader_authStart()

int32_t Bootloader_authStart ( uintptr_t  startAddr,
uint32_t  size 
)

API to start streaming boot authentication.

◆ Bootloader_authUpdate()

int32_t Bootloader_authUpdate ( uintptr_t  startAddr,
uint32_t  size,
uint8_t  enc 
)

API to update the Secure Boot Stream with a new segment.

◆ Bootloader_authFinish()

int32_t Bootloader_authFinish ( void  )

API to finish streaming boot authentication.