AM261x MCU+ SDK  26.00.00
SDL STOG Example

Introduction

The example demonstrates:

  1. Setting a timeout for TOG instance
  2. Error injection for an TOG instance
  3. Error event detection for a timeout event

Use Cases

  • The TOG is programmed with a timeout that is small enough to trigger a timeout event on any access. Error event is triggered and application is notified of the event.

Supported Combinations

Steps to Run the Example

See Also

STOG

Sample Output