This example just does driver and board initialization and prints the string, Hello World! on UART console.
Supported Combinations
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using IAR EW projects to build, import the IAR EW workspace for the required combination and build it using the IAR EW project menu (see Using SDK with IAR Embedded Workbench Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)