AM261x MCU+ SDK  26.00.00
ECAP EDMA Example

Introduction

This example demostrates the ECAP triggerring EDMA for transfer of the ECAP timestamp registers to the TCM location without R5 intervention. ECAP can generate EDMA triggers for Data transfer in both CAPTURE mode and APWM mode

  • In ECAP Capture Mode, the CAPEVTx [x= 1 to 4] can be used and
  • In ECAP APWM Mode, The counter match to Compare or Period can be used.

Example Description:

An ECAP (APWM_ECAP) is configured in APWM mode to generate trigger at its counter matching period event to transfer timestamp data from "CAPTURE_ECAP2". 2 ECAPs (CAPTURE_ECAP1, CAPTURE_ECAP2) are configured to capture the APMW_ECAP PWM wave. CAPTURE_ECAP1 also triggers EDMA on one of its Capture events.

Example Block diagram

ECAP Configurations:

  1. APWM_ECAP:
  • APWM mode, 5KHz and 25% duty cycle
  • DMA trigger at Counter = Period event for channel 0
  • Output routed via Outputxbar13 (GPIO119)
  1. CAPTURE_ECAP1:
  • CAPTURE MODE, capturing Falling, Rising, Falling, Rising edges on its four events,
  • counter resets at CAPEVT1,2,3,4. Thereby, recording
    • ON time at CAP1, CAP3,
    • OFF times at CAP2,CAP4,
  • CAPEVT4 is the source for the DMA channel 1 trigger for the transfer of its timestamps in CAPx
  1. CAPTURE_ECAP2:
  • CAPTURE mode, Capturing Falling, Rising edges on its 2 events,
  • counter resets on CAPEVT1,2. thereby recording,
    • ON time on CAP1
    • OFF time on CAP2 A total of 256 transfers on Channel 0 and 128 transfers on Channel 1 are triggered, and the buffers "capTrigTimeStamps" and "pwmTrigTimeStamps" are compared.

Watch Variables :

  1. capTrigTimeStamps [ ]: array with CAPTURE_ECAP1 Captured timestamps, triggered by Capture mode.
  2. pwmTrigTimeStamps [ ]: array with CAPTURE_ECAP2 Captured timestamps, triggered by APWM mode.

External Connections

AM263X-CC or AM263Px-CC or AM261X-SOM

No external connection is required.

AM263X-LP or AM263Px-LP or AM261X-LP

No external connection is required.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am261x-som, am261x-lp
Example folder examples/drivers/ecap/ecap_edma/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

ECAP

Sample Output

Shown below is a sample output when the application is run,

ECAP triggered EDMA transfers Test Started ...
EDMA transfers complete.
ECAP triggered EDMA transfers Passed!!
All tests have passed!!