AM243x MCU+ SDK  12.01.00

Introduction

UDMA utility API to make TR, get TR descriptor memory requirement.

Go to the source code of this file.

Macros

#define UDMA_GET_TRPD_TR15_SIZE(n)   (UDMA_ALIGN_SIZE(sizeof(CSL_UdmapTR15) + ((n) * (sizeof(CSL_UdmapTR15) + 4U))))
 UDMA TR15 packet descriptor memory size in bytes. This contains the CSL_UdmapCppi5TRPD + Padding to sizeof(CSL_UdmapTR15) + N* Type_15 TR (CSL_UdmapTR15) + N* TR response of 4 bytes. Since CSL_UdmapCppi5TRPD header is less than CSL_UdmapTR15, CSL_UdmapTR15 itself is used for size alignment. More...
 
UDMA TR type

Various UDMA TR type supported

#define UDMA_TR_TYPE_0   (CSL_UDMAP_TR_FLAGS_TYPE_1D_DATA_MOVE)
 
#define UDMA_TR_TYPE_1   (CSL_UDMAP_TR_FLAGS_TYPE_2D_DATA_MOVE)
 
#define UDMA_TR_TYPE_2   (CSL_UDMAP_TR_FLAGS_TYPE_3D_DATA_MOVE)
 
#define UDMA_TR_TYPE_3   (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE)
 
#define UDMA_TR_TYPE_4   (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE_FORMATTING)
 
#define UDMA_TR_TYPE_5   (CSL_UDMAP_TR_FLAGS_TYPE_4D_CACHE_WARM)
 
#define UDMA_TR_TYPE_8   (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE)
 
#define UDMA_TR_TYPE_9   (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING)
 
#define UDMA_TR_TYPE_10   (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE)
 
#define UDMA_TR_TYPE_11   (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE_REPACKING)
 
#define UDMA_TR_TYPE_15   (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING_INDIRECTION)
 

Functions

uint32_t UdmaUtils_getRingMemSize (uint8_t mode, uint32_t elemCnt, uint8_t elemSize)
 UDMA get ring size utility API. More...
 
void UdmaUtils_makeTrpdTr15 (uint8_t *trpdMem, uint32_t trCnt, uint32_t cqRingNum)
 UDMA utility API to make TRPD with TR15 TR type. Other TRPD make APIs should be called only after this API. More...
 
void UdmaUtils_makeTrpd (uint8_t *trpdMem, uint32_t trType, uint32_t trCnt, uint32_t cqRingNum)
 UDMA utility API to make TRPD. Other TRPD make APIs should be called only after this API. More...
 
uint32_t UdmaUtils_getTrSizeEncoded (uint32_t trType)
 Returns the size of TR (encoded) based on the type. More...
 
uint32_t UdmaUtils_getTrSizeBytes (uint32_t trType)
 Returns the size of TR in bytes based on the type. More...
 
static uint32_t UdmaUtils_getTrpdTr15Response (const uint8_t *trpdMem, uint32_t trCnt, uint32_t trIndex)
 Returns the TR response in the TRPD memory based on the index. More...
 
static CSL_UdmapTR15 * UdmaUtils_getTrpdTr15Pointer (uint8_t *trpdMem, uint32_t trIndex)
 Returns the TR15 pointer in the TRPD memory based on the index. More...
 
int32_t UdmaUtils_mapLocaltoGlobalEvent (Udma_DrvHandle drvHandle, Udma_ChHandle chHandle, uint32_t localeventID, uint32_t eventMode)
 Map L2G event for BCDMA trigger. More...