AM243x MCU+ SDK  12.01.00

Detailed Description

Configuration of SA2UL resources.

Parameters
subhdrMagic and size for integrity check
auth_resource_ownerID of the host allowed to acquire/release the authentication resources
enable_saul_psil_global_config_writesFlag for allowing pairing requests from PSIL. Set to 0x5A to enable
safety_host_presentIf safety host is defined. Set to 0x5A to enable
safety_hostID of the host designated as safety host in the system

Data Fields

struct tisci_boardcfg_substructure_header subhdr
 
uint8_t auth_resource_owner
 
uint8_t enable_saul_psil_global_config_writes
 
uint8_t safety_host_present
 
uint8_t safety_host
 

Field Documentation

◆ subhdr

struct tisci_boardcfg_substructure_header tisci_boardcfg_sa2ul_cfg::subhdr

◆ auth_resource_owner

uint8_t tisci_boardcfg_sa2ul_cfg::auth_resource_owner

◆ enable_saul_psil_global_config_writes

uint8_t tisci_boardcfg_sa2ul_cfg::enable_saul_psil_global_config_writes

◆ safety_host_present

uint8_t tisci_boardcfg_sa2ul_cfg::safety_host_present

◆ safety_host

uint8_t tisci_boardcfg_sa2ul_cfg::safety_host