Structure representing the cb_socket_lldcfg_update instance.
Data Fields | |
const char * | dev |
uint16_t | proto |
uint16_t | vlanid |
uint32_t | nTxPkts |
uint32_t | nRxPkts [MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
uint32_t | pktSize |
int | dmaTxChId |
int | dmaRxChId [MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
int | unusedDmaRx |
int | unusedDmaTx |
int | dmaRxShared |
int | dmaRxOwner |
void(* | rxDefaultDataCb )(void *data, int size, int port, void *cbArg) |
void * | rxDefaultCbArg |
uint32_t | numRxChannels |
const char* cb_socket_lldcfg_update_t::dev |
Device name to match the expected socket.
uint16_t cb_socket_lldcfg_update_t::proto |
Protocol or ethernet type in the ethernet frame header to match the expected socket.
uint16_t cb_socket_lldcfg_update_t::vlanid |
VLAN ID to match the expected socket.
uint32_t cb_socket_lldcfg_update_t::nTxPkts |
Number of buffers allocated for transmit packets Positive value will be updated to LLDEnetCfg_t.
uint32_t cb_socket_lldcfg_update_t::nRxPkts[MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
Number of buffers allocated for receive packets Positive value will be updated to LLDEnetCfg_t.
uint32_t cb_socket_lldcfg_update_t::pktSize |
Transmit and receive maximum packet size. Positive value will be updated to LLDEnetCfg_t.
int cb_socket_lldcfg_update_t::dmaTxChId |
DMA transmit channel ID. 0 or positive value will be updated to LLDEnetCfg_t
int cb_socket_lldcfg_update_t::dmaRxChId[MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
DMA receive channel ID. 0 or positive value will be updated to LLDEnetCfg_t
int cb_socket_lldcfg_update_t::unusedDmaRx |
>0: won't use DMA RX; 0: will use DMA RX 0 or positive value will be updated to LLDEnetCfg_t
int cb_socket_lldcfg_update_t::unusedDmaTx |
>0: won't use DMA TX; 0: will use DMA TX 0 or positive value will be updated to LLDEnetCfg_t
int cb_socket_lldcfg_update_t::dmaRxShared |
Only Sitara AM273x support this param. >0: the dmaRxChId is shared between apps; 0: not shared 0 or positive value will be updated to LLDEnetCfg_t
int cb_socket_lldcfg_update_t::dmaRxOwner |
Only Sitara AM273x support this param. >0: the socket owns this RX DMA channel; 0: not own 0 or positive value will be updated to LLDEnetCfg_t
Only Sitara AM273x support this param. Default RX data callback when there is no matching RX filter.
void* cb_socket_lldcfg_update_t::rxDefaultCbArg |
Only Sitara AM273x support this param. Default RX data callback arg
uint32_t cb_socket_lldcfg_update_t::numRxChannels |
Number of Rx DMA channels, only ICSSG peripheral has more than 1 Rx DMA channels.