AM243x MCU+ SDK  12.01.00
SDL_R5ExptnHandlers Struct Reference

Detailed Description

Structure containing the Exception Handlers. If application does not want register an exception handler then below handlers can be assigned to 'NULL' value. In such case, default handler will be used which have the infinite loop.

Data Fields

exptnHandlerPtr udefExptnHandler
 
void * udefExptnHandlerArgs
 
exptnHandlerPtr swiExptnHandler
 
void * swiExptnHandlerArgs
 
exptnHandlerPtr pabtExptnHandler
 
void * pabtExptnHandlerArgs
 
exptnHandlerPtr dabtExptnHandler
 
void * dabtExptnHandlerArgs
 
exptnHandlerPtr irqExptnHandler
 
void * irqExptnHandlerArgs
 
exptnHandlerPtr fiqExptnHandler
 
void * fiqExptnHandlerArgs
 

Field Documentation

◆ udefExptnHandler

exptnHandlerPtr SDL_R5ExptnHandlers::udefExptnHandler

Undefined Instruction exception handler

◆ udefExptnHandlerArgs

void* SDL_R5ExptnHandlers::udefExptnHandlerArgs

Undefined Instruction exception handler Args

◆ swiExptnHandler

exptnHandlerPtr SDL_R5ExptnHandlers::swiExptnHandler

Software Interrupt exception handler

◆ swiExptnHandlerArgs

void* SDL_R5ExptnHandlers::swiExptnHandlerArgs

Software Interrupt exception handler Args

◆ pabtExptnHandler

exptnHandlerPtr SDL_R5ExptnHandlers::pabtExptnHandler

Prefetch Abort exception handler

◆ pabtExptnHandlerArgs

void* SDL_R5ExptnHandlers::pabtExptnHandlerArgs

Prefetch Abort exception handler Args

◆ dabtExptnHandler

exptnHandlerPtr SDL_R5ExptnHandlers::dabtExptnHandler

Data Abort exception handler

◆ dabtExptnHandlerArgs

void* SDL_R5ExptnHandlers::dabtExptnHandlerArgs

Data Abort exception handler Args

◆ irqExptnHandler

exptnHandlerPtr SDL_R5ExptnHandlers::irqExptnHandler

Interrupt Request exception handler. This will be used only if VIM is not enabled.

◆ irqExptnHandlerArgs

void* SDL_R5ExptnHandlers::irqExptnHandlerArgs

Interrupt Request exception handler Args. This will be used only if VIM is not enabled.

◆ fiqExptnHandler

exptnHandlerPtr SDL_R5ExptnHandlers::fiqExptnHandler

Fast Interrupt Request exception handler. This will be used only if VIM is not enabled.

◆ fiqExptnHandlerArgs

void* SDL_R5ExptnHandlers::fiqExptnHandlerArgs

Fast Interrupt Request exception handler Args. This will be used only if VIM is not enabled.