AM243x MCU+ SDK  12.01.00
MMCSD_EmmcDeviceData Struct Reference

Detailed Description

eMMC device properties

Data Fields

uint32_t ocr
 
uint32_t rca
 
uint16_t maxReadBlockLen
 
uint16_t maxWriteBlockLen
 
char manuDate [9]
 
uint8_t manuID
 
char productName [7]
 
uint8_t specVersion
 
uint32_t blockCount
 
uint8_t transferSpeed
 
uint8_t supportedModes
 
uint8_t eStrobeSupport
 
uint8_t driveStrength
 
bool isHC
 

Field Documentation

◆ ocr

uint32_t MMCSD_EmmcDeviceData::ocr

Operating conditions register Value

◆ rca

uint32_t MMCSD_EmmcDeviceData::rca

Relative card address

◆ maxReadBlockLen

uint16_t MMCSD_EmmcDeviceData::maxReadBlockLen

Maximum supported block length for read

◆ maxWriteBlockLen

uint16_t MMCSD_EmmcDeviceData::maxWriteBlockLen

Maximum supported block length for write

◆ manuDate

char MMCSD_EmmcDeviceData::manuDate[9]

ASCII string with the date of manufacture

◆ manuID

uint8_t MMCSD_EmmcDeviceData::manuID

Card manufacturer ID

◆ productName

char MMCSD_EmmcDeviceData::productName[7]

Product name

◆ specVersion

uint8_t MMCSD_EmmcDeviceData::specVersion

eMMC specification version

◆ blockCount

uint32_t MMCSD_EmmcDeviceData::blockCount

Number of blocks in the eMMC

◆ transferSpeed

uint8_t MMCSD_EmmcDeviceData::transferSpeed

Transfer speed in code - Freq Unit x Mult Factor

◆ supportedModes

uint8_t MMCSD_EmmcDeviceData::supportedModes

Supported speed modes by the device - HS200, HS400 etc

◆ eStrobeSupport

uint8_t MMCSD_EmmcDeviceData::eStrobeSupport

Support of enhanced strobe

◆ driveStrength

uint8_t MMCSD_EmmcDeviceData::driveStrength

Drive strength of the device

◆ isHC

bool MMCSD_EmmcDeviceData::isHC

Card whether high Capacity or not