AM243x MCU+ SDK  12.01.00
GPTIMER_HwAttrs Struct Reference

Detailed Description

GPTIMER Hardware attributes.

Data Fields

uint32_t baseAddr
 
uint32_t intNum
 
uint16_t eventId
 
uint32_t inputClk
 
bool enableIntr
 
uint8_t intrPriority
 

Field Documentation

◆ baseAddr

uint32_t GPTIMER_HwAttrs::baseAddr

TIMER Peripheral base address

◆ intNum

uint32_t GPTIMER_HwAttrs::intNum

TIMER Peripheral interrupt vector

◆ eventId

uint16_t GPTIMER_HwAttrs::eventId

TIMER Peripheral event id

◆ inputClk

uint32_t GPTIMER_HwAttrs::inputClk

TIMER input input clock

◆ enableIntr

bool GPTIMER_HwAttrs::enableIntr

Enable Interrupt

◆ intrPriority

uint8_t GPTIMER_HwAttrs::intrPriority

Interrupt Priority