AM243x MCU+ SDK  12.01.00
Enet_MacDstFlowInfo Struct Reference

Detailed Description

Output args for ENET_PER_IOCTL_ATTACH_CORE command.

Data Fields

uint32_t coreKey
 
uint32_t startIdx
 
uint32_t flowIdx
 
uint8_t macAddress [ENET_MAC_ADDR_LEN]
 

Field Documentation

◆ coreKey

uint32_t Enet_MacDstFlowInfo::coreKey

Core Key

◆ startIdx

uint32_t Enet_MacDstFlowInfo::startIdx

Rx Flow Base or Start index

◆ flowIdx

uint32_t Enet_MacDstFlowInfo::flowIdx

Allocated flow's index (offset from startIdx)

◆ macAddress

uint8_t Enet_MacDstFlowInfo::macAddress[ENET_MAC_ADDR_LEN]

Destination mac address associated with the flow