AM243x MCU+ SDK  12.01.00
EnetUdma_UdmaFlowPrms Struct Reference

Detailed Description

UDMA RX channel flow parameters.

The structure is stripped down version of Udma_FlowPrms.

Data Fields

uint8_t einfoPresent
 
uint8_t psInfoPresent
 
uint16_t sopOffset
 
uint16_t defaultRxCQ
 
uint8_t sizeThreshEn
 

Field Documentation

◆ einfoPresent

uint8_t EnetUdma_UdmaFlowPrms::einfoPresent

[IN] Set to 1 if extended packet info is present in the descriptor

◆ psInfoPresent

uint8_t EnetUdma_UdmaFlowPrms::psInfoPresent

[IN] Set to 1 if protocol-specific info is present in the descriptor

◆ sopOffset

uint16_t EnetUdma_UdmaFlowPrms::sopOffset

[IN] Start of rx packet data (byte offset from the start of the SOP buffer)

◆ defaultRxCQ

uint16_t EnetUdma_UdmaFlowPrms::defaultRxCQ

[IN] RX destination queue

◆ sizeThreshEn

uint8_t EnetUdma_UdmaFlowPrms::sizeThreshEn

[IN] UDMAP receive flow packet size based free buffer queue enable configuration