AM243x MCU+ SDK  12.01.00

Detailed Description

PHY driver object.

Data Fields

EnetPhy_MdioHandle hMdio
 
EnetPhy_Cfg phyCfg
 
EnetPhy_Mii mii
 
uint32_t macCaps
 
EnetPhy_LinkCfg linkCfg
 
EnetPhy_FsmTimeoutCfg timeoutCfg
 
EnetPhy_State state
 
uint32_t group
 
uint32_t addr
 
uint32_t reqLinkCaps
 
Phy_DrvObj_t hDrvIf
 
EnetPhy_Magic magic
 
Mdio_Obj * mdioArgs
 
void * priv
 

Field Documentation

◆ hMdio

EnetPhy_MdioHandle EnetPhy_Obj::hMdio

MDIO handle used to access PHY registers

◆ phyCfg

EnetPhy_Cfg EnetPhy_Obj::phyCfg

PHY configuration params

◆ mii

EnetPhy_Mii EnetPhy_Obj::mii

MII interface type

◆ macCaps

uint32_t EnetPhy_Obj::macCaps

MAC port supported capabilities

◆ linkCfg

EnetPhy_LinkCfg EnetPhy_Obj::linkCfg

Port Link configuration (speed, duplexity)

◆ timeoutCfg

EnetPhy_FsmTimeoutCfg EnetPhy_Obj::timeoutCfg

State-machine timeout configuration

◆ state

EnetPhy_State EnetPhy_Obj::state

State-machine state

◆ group

uint32_t EnetPhy_Obj::group

PHY group

◆ addr

uint32_t EnetPhy_Obj::addr

PHY device address

◆ reqLinkCaps

uint32_t EnetPhy_Obj::reqLinkCaps

Requested link capability mask

◆ hDrvIf

Phy_DrvObj_t EnetPhy_Obj::hDrvIf

PHY driver

◆ magic

EnetPhy_Magic EnetPhy_Obj::magic

Magic number indicating that this object is in use

◆ mdioArgs

Mdio_Obj* EnetPhy_Obj::mdioArgs

Caller-provided arguments to be used in MDIO driver calls

◆ priv

void* EnetPhy_Obj::priv

Private data that is used by the driver