AM243x MCU+ SDK  12.01.00
CANFD_MessageObject Struct Reference

Data Fields

uint32_t startMsgId
 Starting range of the Message Id to which the configuration belongs. For Tx and single Message Id objects the startMsgId = endMsgId. More...
 
uint32_t endMsgId
 Ending range of the Message Id to which the configuration belongs For Tx and single Message Id objects the startMsgId = endMsgId. More...
 
CANFD_Config * canfdHandle
 Pointer to the CANFD driver object. More...
 
CANFD_Direction direction
 Message object direction. More...
 
CANFD_MCANXidType msgIdType
 Message object type. More...
 
uint32_t messageObjNum
 Allocated message object number. More...
 
uint32_t dataLength
 Data Length used by application for transmission and reception. Valid values: 1 to 64 bytes. More...
 
uint32_t txElement
 Tx buffer number used to send data. More...
 
uint32_t rxElement
 Rx buffer number used to receive data. More...
 
MCAN_MemType txMemType
 Part of message ram to accessed by this message object. Refer enum MCAN_MemType. More...
 
MCAN_MemType rxMemType
 Part of message ram to accessed by this message object. Refer enum MCAN_MemType. More...
 
uint32_t rxFifoNum
 FIFO Num (MCAN_RX_FIFO_NUM_0/MCAN_RX_FIFO_NUM_1). More...
 
uint32_t interruptsRxed
 Number of interrupts received. More...
 
uint32_t messageProcessed
 Number of messages processed. More...
 
uint32_t dmaEventNo
 Dma Event number allocated for this message object. More...
 
CANFD_DmaMsgConfig dmaMsgConfig
 Dma message configuration. More...
 
void * args
 Pointer to be used by application to store rx buffer. More...
 
void * filterConfig
 void pointer to MCAN_ExtMsgIDFilterElement or MCAN_StdMsgIDFilterElement structure. It will point
to any of the two structure based on fdMode. More...
 

Field Documentation

◆ startMsgId

uint32_t CANFD_MessageObject::startMsgId

Starting range of the Message Id to which the configuration belongs. For Tx and single Message Id objects the startMsgId = endMsgId.

◆ endMsgId

uint32_t CANFD_MessageObject::endMsgId

Ending range of the Message Id to which the configuration belongs For Tx and single Message Id objects the startMsgId = endMsgId.

◆ canfdHandle

CANFD_Config* CANFD_MessageObject::canfdHandle

Pointer to the CANFD driver object.

◆ direction

CANFD_Direction CANFD_MessageObject::direction

Message object direction.

◆ msgIdType

CANFD_MCANXidType CANFD_MessageObject::msgIdType

Message object type.

◆ messageObjNum

uint32_t CANFD_MessageObject::messageObjNum

Allocated message object number.

◆ dataLength

uint32_t CANFD_MessageObject::dataLength

Data Length used by application for transmission and reception. Valid values: 1 to 64 bytes.

◆ txElement

uint32_t CANFD_MessageObject::txElement

Tx buffer number used to send data.

◆ rxElement

uint32_t CANFD_MessageObject::rxElement

Rx buffer number used to receive data.

◆ txMemType

MCAN_MemType CANFD_MessageObject::txMemType

Part of message ram to accessed by this message object. Refer enum MCAN_MemType.

◆ rxMemType

MCAN_MemType CANFD_MessageObject::rxMemType

Part of message ram to accessed by this message object. Refer enum MCAN_MemType.

◆ rxFifoNum

uint32_t CANFD_MessageObject::rxFifoNum

FIFO Num (MCAN_RX_FIFO_NUM_0/MCAN_RX_FIFO_NUM_1).

◆ interruptsRxed

uint32_t CANFD_MessageObject::interruptsRxed

Number of interrupts received.

◆ messageProcessed

uint32_t CANFD_MessageObject::messageProcessed

Number of messages processed.

◆ dmaEventNo

uint32_t CANFD_MessageObject::dmaEventNo

Dma Event number allocated for this message object.

◆ dmaMsgConfig

CANFD_DmaMsgConfig CANFD_MessageObject::dmaMsgConfig

Dma message configuration.

◆ args

void* CANFD_MessageObject::args

Pointer to be used by application to store rx buffer.

◆ filterConfig

void* CANFD_MessageObject::filterConfig

void pointer to MCAN_ExtMsgIDFilterElement or MCAN_StdMsgIDFilterElement structure. It will point
to any of the two structure based on fdMode.