AM243x MCU+ SDK  12.01.00
sdl_lbist.h File Reference

Go to the source code of this file.

Enumerations

enum  SDL_LBIST_testType { SDL_LBIST_TEST, SDL_LBIST_TEST_RELEASE, SDL_LBIST_TEST_INVALID }
 LBIST self test type. More...
 

Functions

int32_t SDL_LBIST_selfTest (SDL_LBIST_inst instance, SDL_LBIST_testType testType)
 LBIST self test. More...
 
int32_t SDL_LBIST_checkResult (SDL_LBIST_inst instance, bool *pResult)
 Check the result of the LBIST test. More...
 
uint8_t SDL_LBIST_checkDone (SDL_LBIST_inst instance)
 Check the status of the LBIST test. More...